BLE_TRSPS_SendVendorCommand
C
uint16_t BLE_TRSPS_SendVendorCommand(uint16_t connHandle, uint8_t commandID, uint8_t commandLength, uint8_t *p_commandPayload);
Description
Sends a vendor-specific command over BLE.
Parameters
Parameter | Description |
---|---|
[in] connHandle | Connection handle associated with this connection. |
[in] commandID | The identifier of the vendor-specific command. |
[in] commandLength | The length of the command payload. |
[in] p_commandPayload | Pointer to the command payload data. |
Return values
Return value | Description |
---|---|
MBA_RES_SUCCESS | Command successfully sent. |
MBA_RES_FAIL | Failed due to an invalid connection handle. |
MBA_RES_OOM | Internal memory allocation failure. |
MBA_RES_INVALID_PARA | Invalid parameters; incorrect commandID, commandLength, or CCCD of TCP not enabled. |