BLE_TRCBPS_SendData
C
uint16_t BLE_TRCBPS_SendData(uint16_t connHandle, uint16_t len, uint8_t *p_data);
Description
Send data through the BLE Transparent Credit Based Profile Data pipe.
Parameters
Parameter | Description |
---|---|
[in] connHandle | Connection handle. |
[in] len | Length of the data to be sent. Must not exceed BLE_TRCBPS_DATA_MTU. |
[in] p_data | Pointer to the buffer containing the data to send. |
Return values
Return value | Description |
---|---|
MBA_RES_BAD_STATE | Connection not established. |