BLE_DTM_EnhancedReceiverTest
C
uint16_t BLE_DTM_EnhancedReceiverTest(uint8_t rxChannel, uint8_t phy);Description
Starts a receiver test where the device receives test reference packets at a fixed interval.
Note
BLE_DTM_Init must be called before using this function.
Parameters
| Parameter | Description |
|---|---|
| [in] rxChannel | Channel number calculated as (F – 2402) / 2, where F is the frequency in MHz ranging from 2402 to 2480 MHz. See Receiver or transmitter channel range for the valid ranges. |
| [in] phy | PHY type setting for the test. See Receiver PHY types for possible values. |
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | Successfully starts the receiver test. |
| MBA_RES_OOM | Internal memory allocation failure occurred. |
| MBA_RES_INVALID_PARA | The provided parameters are invalid. |