BLE_TRSPS_GetData
C
uint16_t BLE_TRSPS_GetData(uint16_t connHandle, uint8_t *p_data);Description
Retrieves queued data from the profile.
Parameters
| Parameter | Description |
|---|---|
| [in] connHandle | Connection handle associated with the queued data. |
| [out] p_data | Pointer to the buffer where the data will be stored. |
Return values
| Return value | Description |
|---|---|
| MBA_RES_SUCCESS | Data successfully retrieved. |
| MBA_RES_FAIL | No data in the queue or the connection link could not be found. |