STACK_Event_T
C
typedef struct STACK_Event_T
{
STACK_GroupId_T groupId;
uint16_t evtLen;
uint8_t *p_event;
} STACK_Event_T;Description
Structure representing an event generated by the STACK.
Field Documentation
| Field | Description |
|---|---|
| groupId | Identifier for the group to which the event belongs. Refer to STACK_GroupId_T for possible values. |
| evtLen | The length of the event data in bytes. |
| p_event | A pointer to the event data. This is the actual information related to the event that occurred within the STACK. |