22.2 PPS Inputs

Each digital peripheral has a dedicated PPS Peripheral Input Selection (xxxPPS) register, with which the input pin to the peripheral is selected. Devices that have 20 leads or less (8/14/16/20) allow PPS routing to any I/O pin, while devices with 28 leads or more allow PPS routing to I/Os contained within two ports, with the exception of the following signals, which are routed to three ports:
  • SPI1SCKPPS
  • SPI1SDIPPS
  • I2C1SCLPPS
  • I2C1SDAPPS
  • CLBINxPPS
  • CLBCLKPPS

The outputs of the Signal Routing Port (SRPORT) can also be used as inputs to other peripherals using PPS (see the table below).

Important: The notation “xxx” in the generic register name is a placeholder for the peripheral identifier. For example, xxx = T0CKI for the T0CKIPPS register.

Multiple peripherals can operate from the same source simultaneously. Port reads always return the pin level regardless of peripheral PPS selection. If a pin also has analog functions associated, the ANSEL bit for that pin must be cleared to enable the digital input buffer.

Table 22-1. PPS Input Selection Table
PeripheralPPS Input RegisterDefault Pin Selection at PORRegister Reset Value at PORAvailable Input Port
CLBOUTL/H28-Pin Devices40-Pin Devices48-Pin Devices
Interrupt 0INT0PPSRB0‘b0000 1000CLBOUTLABWABWABW
Interrupt 1INT1PPSRB1‘b0000 1001CLBOUTLABWABWBDW
Interrupt 2INT2PPSRB2‘b0000 1010CLBOUTLABWABWBFW
Timer0 ClockT0CKIPPSRA4‘b0000 0100CLBOUTHABWABWAFW
Timer1 ClockT1CKIPPSRC0‘b0001 0000CLBOUTHACWACWCEW
Timer1 GateT1GPPSRB5‘b0000 1101CLBOUTHBCWBCWBCW
Timer3 ClockT3CKIPPSRC0‘b0001 0000CLBOUTLBCWBCWCEW
Timer3 GateT3GPPSRC0‘b0001 0000CLBOUTLACWACWACW
Timer2 InputT2INPPSRC3‘b0001 0011CLBOUTHACWACWACW
Timer4 InputT4INPPSRC5‘b0001 0101CLBOUTHBCWBCWBCW
Universal Timer Input 0TUIN0PPSRC0‘b0001 0000CLBOUTHACWCEWCEW
Universal Timer Input 1TUIN1PPSRB5‘b0000 1101CLBOUTHBCWBCWBFW
CCP1CCP1PPSRC2‘b0001 0010CLBOUTLBCWBCWCFW
PWM Input 0PWMIN0PPSRC2‘b0001 0010CLBOUTLBCWBCWCFW
PWM Input 1PWMIN1PPSRC1‘b0001 0001CLBOUTLBCWBCWCFW
PWM1 External Reset SourcePWM1ERSPPSRC3‘b0001 0011CLBOUTLACWACWAC W
PWM2 External Reset SourcePWM2ERSPPSRC5‘b0001 0101CLBOUTLACWACWCEW
CWG1CWG1PPSRB0‘b0000 1000CLBOUTLBCBDBD
CLCx Input 1CLCIN0PPSRA0‘b0000 0000CLBOUTL/HACWACWACW
CLCx Input 2CLCIN1PPSRA1‘b0000 0001CLBOUTL/HACWACWACW
CLCx Input 3CLCIN2PPSRB6‘b0000 1110CLBOUTL/HBCWBDWBDW
CLCx Input 4CLCIN3PPSRB7‘b0000 1111CLBOUTL/HBCWBDWBDW
CLCx Input 5CLCIN4PPSRA0‘b0000 0000CLBOUTL/HACWACWACW
CLCx Input 6CLCIN5PPSRA1‘b0000 0001CLBOUTL/HACWACWACW
CLCx Input 7CLCIN6PPSRB6‘b0000 1110CLBOUTL/HBCWBDWBDW
CLCx Input 8CLCIN7PPSRB7‘b0000 1111CLBOUTL/HBCWBDWBDW
ADC Conversion TriggerADACTPPSRB4‘b0000 1100CLBOUTHBCWBDWBDW
SPI1 ClockSPI1SCKPPSRC3‘b0001 0011CLBOUTHBCWBCDWBCDW
SPI1 DataSPI1SDIPPSRC4‘b0001 0100CLBOUTHBCWBCDWBCDW
SPI1 Client SelectSPI1SSPPSRA5‘b0000 0101CLBOUTHACWADWADW
I2C1 ClockI2C1SCLPPS(1)RC3‘b0001 0011CLBOUTHBCBCDBCD
I2C1 DataI2C1SDAPPS(1)RC4‘b0001 0100CLBOUTHBCBCDBCD
UART1 ReceiveU1RXPPSRC5‘b0001 0101CLBOUTHBCWBCWCFW
UART1 Clear to SendU1CTSPPSRC6‘b0001 0110CLBOUTHBCBCCF
UART2 ReceiveU2RXPPSRB7‘b0000 1111CLBOUTHBCWBDWBDW
UART2 Clear to SendU2CTSPPSRB6‘b0000 1110CLBOUTHBCBDBD
Signal Routing Port Input 0PORTWIN0PPSRB2‘b0000 1010CLBOUTLABBDBD
Signal Routing Port Input 1PORTWIN1PPSRB0‘b0000 1000CLBOUTLABBDBD
Signal Routing Port Clock InputPORTWCLKPPSRB1‘b0000 1001CLBOUTLABBDBD
DSM Modulation Carrier HighMD1CARLPPSRA3‘b0000 0011CLBOUTL/HACWADWADW
DSM Modulation Carrier LowMD1CARHPPSRA4‘b0000 0100CLBOUTL/HACWADWADW
DSM Modulation SourceMD1SRCPPSRA5‘b0000 0101CLBOUTL/HACWADWADW
CLB Input 0CLBIN0PPSRC0‘b0001 0000ACACDACD
CLB Input 1CLBIN1PPSRC1‘b0001 0001ACACDACD
CLB Input 2CLBIN2PPSRC2‘b0001 0010ACACDACD
CLB Input 3CLBIN3PPSRC3‘b0001 0011ACACDACD
CLB Input 4CLBIN4PPSRC4‘b0001 0100ACACDACD
CLB Input 5CLBIN5PPSRC5‘b0001 0101ACACDACD
CLB Input 6CLBIN6PPSRC6‘b0001 0110ACACDACD
CLB Input 7CLBIN7PPSRA0‘b0000 0000ACACDACD
CLB ClockCLBCLKPPSRA1‘b0000 0001ACACDACD
Note:
  1. Bidirectional pin. The corresponding output must select the same pin.