1 Harmony 3 Peripheral Library Application Examples for PIC32MZ DA Family
The following applications are provided to demonstrate the typical or interesting usage models of one or more peripheral libraries.
| Name | Description |
|---|---|
| ADCHS DMA | This example application shows how to sample an analog input using the ADCHS peripheral and displays the converted samples on a serial terminal. |
| ADCHS Interrupt | This example application shows how to sample an analog input using the ADCHS peripheral and displays the converted samples on a serial terminal |
| ADCHS Polling | This example application shows how to sample an analog input using the ADCHS peripheral and displays the converted samples on a serial terminal |
| Cache Maintenance Operations | This example demonstrates the cache maintenance operation by cleaning and invalidating the cache for the DMA buffers located in the cacheable SRAM region |
| CMP Configurable Reference | This example application shows how to use the CMP Peripheral library to compare voltage level on the negative input with the internal configurable reference voltage |
| CORETIMER Periodic Interrupt | This example application shows how to use the CoreTimer to generate periodic interrupts |
| DMAC Memory Transfer | This example application demonstrates how to use the DMAC peripheral to do a memory to memory transfer |
| DMAC USART Echo | This example application demonstrates USART transfer with DMA to receive 10 bytes and echo back the received bytes |
| DMT Timeout | This example application shows how the deadman timer resets by not clearing the deadman timer counter on switch press |
| GPIO Interrupt | This example application demonstrate how to generate GPIO interrupt on switch press and release, and indicate the switch status using the LED |
| GPIO Polling | This example application demonstrate how to poll the switch input, and indicate the switch status using the LED |
| I2C EEPROM Read Write | This example application demonstrates how to use the I2C peripheral to write and read from the I2C serial EEPROM memory |
| ICAP Capture Mode | This example application shows how to use the ICAP peripheral to measure the pulse width of the input signal |
| NVM Flash Read Write | This example application demonstrates how to use the NVM to erase and program the internal Flash memory |
| OCMP Compare Mode | This example application shows how to use the OCMP peripheral to generate an active low, active high, and toggle output on compare match |
| RNG Random Number | This example application shows how to use the RNG Peripheral library to generate a pseudo-random number |
| RTCC Alarm Interrupt | This example application shows how to use the RTCC to configure the time and generate the alarm |
| SPI Blocking | This example application demonstrates how to use the SPI peripheral to transmit and receive a block of data in a blocking manner |
| SPI Interrupt | This example application demonstrates how to use the SPI peripheral to transmit and receive a block of data using interrupt |
| SQI Flash Read Write | This example application demonstrates how to use the SQI Peripheral library to perform erase, write and read operation with the SQI Serial Flash memory |
| TMR Periodic Interrupt | This example demonstrates how to use the TMR module in timer mode to generate periodic interrupt |
| TMR1 Periodic Interrupt | This example demonstrates how to use the TMR1 module in timer mode to generate periodic interrupt |
| UART Echo Blocking | This example application demonstrates how to use the UART peripheral to transfer a block of data in a blocking manner |
| UART Echo Interrupt | This example application demonstrates how to use the UART peripheral to transfer a block of data in a non-blocking manner |
| UART Ring Buffer | This example application demonstrates how to use the UART peripheral in ring buffer mode |
| WDT Timeout | This example application shows how the watchdog timer resets by not feeding the watchdog on switch press |