Perform the following procedure to update a core
version:
Download the latest version of the core into your vault.
Upgrade each configured core in your design to the latest version by
right-clicking the core component in the design hierarchy and selecting
Update Component Version. The component is
regenerated automatically.
Important: The Update Component
Version option is now available on instances of core
components in a SmartDesign canvas as well. In addition, the selected core
version is downloaded automatically from the Update Component Version dialog
itself if needed.
Review the SmartDesign components and user RTL files in which the core
component has been instantiated. If the port-list of the core component is
modified after updating to the new core version, right-click the core
component's instance in the SmartDesign and select Update
Instance to update its port-list. Check for any pin/port
disconnections in the SmartDesign or for any new pins exposed on the core
component's instance, and then connect them or tie them off as needed and
regenerate the SmartDesign component.
Build Design Hierarchy and Derive the Timing Constraints again from the
Constraint Manager tool to use the latest generated core timing
constraints.
Rerun the design flow.
Rev: C
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.