8.2 Pin Description

The device features several PIO controllers that multiplex the I/O lines of the peripheral set. Table 8-1 defines how the I/O lines are multiplexed on the different PIO controllers. The "Reset State" column shows whether the PIO line resets in I/O mode or in Peripheral mode. If I/O is shown, the PIO line resets with the characteristics (input, output, pull-up or pull-down) indicated in this same column, so that the device is configured in a known state as soon as the reset is released. As a result, PIO_CFGR.FUNC resets to ‘0’. If a signal name is shown in the “Reset State” column, the PIO line is assigned to this function and PIO_CFGR.FUNC is not set to ‘0’. That is the case for pins controlling memories, in particular address lines, which require the pin to be driven as soon as the reset is released.

Table 8-1. Pin Description(1)(2)

427-pin
TFBGA

Power
Rail

I/O
Type

(3)
PrimaryAlternatePIO PeripheralReset State
SignalDirSignalDirFuncSignalDirI/O Set

Signal, Dir,

PU, PD,

HiZ, ST(4)

W21VDDSDMMC0HSIOPA0I/OASDMMC0_CKO1PIO, I, PU, ST
BFLEXCOM3_IO0I/O1
CNWE/NWR0/NANDWEO1
AA19VDDSDMMC0HSIOPA1I/OASDMMC0_CMDI/O1PIO, I, PU, ST
BFLEXCOM3_IO1I/O1
CA21/NANDALEO1,2
W19VDDSDMMC0HSIOPA2I/OASDMMC0_RSTNO1PIO, I, PU, ST
BFLEXCOM3_IO2I/O1
CA22/NANDCLEO1,2
Y19VDDSDMMC0HSIOPA3I/OASDMMC0_DAT0I/O1PIO, I, PU, ST
BFLEXCOM3_IO3I/O1
CD0I/O1
W20VDDSDMMC0HSIOPA4I/OASDMMC0_DAT1I/O1PIO, I, PU, ST
BFLEXCOM3_IO4O1
CD1I/O1
AA18VDDSDMMC0HSIOPA5I/OASDMMC0_DAT4I/O1PIO, I, PU, ST
BFLEXCOM2_IO0I/O3
CD4I/O1
FTCLK4I3
U19VDDSDMMC0HSIOPA6I/OASDMMC0_DAT5I/O1PIO, I, PU, ST
BFLEXCOM2_IO1I/O3
CD5I/O1
FTIOB4I/O3
AA17VDDSDMMC0HSIOPA7I/OASDMMC0_DAT6I/O1PIO, I, PU, ST
BFLEXCOM2_IO2I/O3
CD6I/O1
FTIOA4I/O3
T18VDDSDMMC0HSIOPA8I/OASDMMC0_DAT7I/O1PIO, I, PU, ST
BFLEXCOM2_IO3I/O3
CD7I/O1
FTIOA5I/O3
AA16VDDSDMMC0HSIOPA9I/OASDMMC0_DAT2I/O1PIO, I, PU, ST
BFLEXCOM0_IO2I/O1
CD2I/O1
FTIOB5I/O3
W17VDDSDMMC0HSIOPA10I/OASDMMC0_DAT3I/O1PIO, I, PU, ST
BFLEXCOM0_IO3I/O1
CD3I/O1
FTCLK5I3
V17VDDSDMMC0HSIOPA11I/OASDMMC0_DSI1PIO, I, PU, ST
BFLEXCOM0_IO4O1
CNANDRDYI1,2
FTIOB3I/O3
Y17VDDSDMMC0HSIOPA12I/OBFLEXCOM0_IO0I/O1PIO, I, PU, ST
CNRD/NANDOEO1,2
DPCK0O1
EEXT_IRQ0I1
FTIOA3I/O3
U17VDDSDMMC0HSIOPA13I/OBFLEXCOM0_IO1I/O1PIO, I, PU, ST
CNCS0/NANDCS0O1,2
DPCK1O1
FTCLK3I3
W13VDDIOP0GPIOPA14I/OAFLEXCOM4_IO4O1PIO, I, PU, ST
BSDMMC0_WPI1
CFLEXCOM3_IO0I/O4
P15VDDIOP0GPIOPA15I/OAFLEXCOM4_IO3I/O1PIO, I, PU, ST
BSDMMC0_1V8SELO1
CFLEXCOM3_IO1I/O4
V11VDDIOP0GPIOPA16I/OAFLEXCOM4_IO2I/O1PIO, I, PU, ST
BSDMMC0_CDI1
DPCK2O1
EEXT_IRQ1I1
R17VDDIOP0GPIOPA17I/OAFLEXCOM4_IO1I/O1PIO, I, PU, ST
U11VDDIOP0GPIOPA18I/OAFLEXCOM4_IO0I/O1PIO, I, PU, ST
V13VDDIOP0GPIOPA19I/OATK0I/O1PIO, I, PU, ST
CFLEXCOM4_IO5O1
DPWML0O3
T17VDDIOP0GPIOPA20I/OATD0O1PIO, I, PU, ST
BFLEXCOM3_IO4O2
CFLEXCOM4_IO6O1
DPWMH0O3
U13VDDIOP0GPIOPA21I/OATF0I/O1PIO, I, PU, ST
BFLEXCOM3_IO3I/O2
DPWML1O3
R15VDDIOP0GPIOPA22I/OARD0I1PIO, I, PU, ST
BFLEXCOM3_IO2I/O2
CPDMC0_DS1I1
DPWMH1O3
U15VDDIOP0GPIOPA23I/OARK0I/O1PIO, I, PU, ST
BFLEXCOM3_IO1I/O2
CPDMC0_CLKO1
DPWML2O3
T13VDDIOP0GPIOPA24I/OARF0I/O1PIO, I, PU, ST
BFLEXCOM3_IO0I/O2
CPDMC0_DS0I1
DPWMH2O3
R24VDDGMAC0GPIOPA25I/OAG0_TXCTL/G0_TXENO1,2PIO, I, PU, ST
BFLEXCOM6_IO2I/O1
R23VDDGMAC0GPIOPA26I/OAG0_TX0O1,2PIO, I, PU, ST
BFLEXCOM6_IO3I/O1
N24VDDGMAC0GPIOPA27I/OAG0_TX1O1,2PIO, I, PU, ST
BFLEXCOM6_IO4O1
L21VDDGMAC0GPIOPA28I/OAG0_RXCTL/G0_CRSDVI1,2PIO, I, PU, ST
BFLEXCOM6_IO0I/O1
M25VDDGMAC0GPIOPA29I/OAG0_RX0I1,2PIO, I, PU, ST
BFLEXCOM6_IO1I/O1
N23VDDGMAC0GPIOPA30I/OAG0_RX1I1,2PIO, I, PU, ST
BFLEXCOM8_IO0I/O1
N25VDDGMAC0GPIOPA31I/OAG0_MDCO1,2PIO, I, PU, ST
BFLEXCOM8_IO1I/O1
L20VDDGMAC0GPIOPB0I/OAG0_MDIOI/O1,2PIO, I, PU, ST
BFLEXCOM8_IO3I/O1
P25VDDGMAC0GPIOPB1I/OAG0_REFCK/G0_TXCKI/O2,1PIO, I, PU, ST
BFLEXCOM8_IO2I/O1
L23VDDGMAC0GPIOPB2I/OAG0_RX2I1PIO, I, PU, ST
BFLEXCOM8_IO4O1
CG0_RXERI2
DRK0I/O2
R25VDDGMAC0GPIOPB3I/OAG0_RXCKI1PIO, I, PU, ST
BFLEXCOM10_IO2I/O2
DTK0I/O2
L24VDDGMAC0GPIOPB4I/OAG0_TX2O1PIO, I, PU, ST
BFLEXCOM10_IO3I/O2
DTF0I/O2
T25VDDGMAC0GPIOPB5I/OAG0_TX3O1PIO, I, PU, ST
BFLEXCOM10_IO4O2
DTD0O2
L19VDDGMAC0GPIOPB6I/OAG0_RX3I1PIO, I, PU, ST
BFLEXCOM10_IO0I/O2
DRD0I2
U25VDDGMAC0GPIOPB7I/OAG0_TSUCOMPO1,2PIO, I, PU, ST
BFLEXCOM10_IO1I/O2
CADTRGI1
DRF0I/O2
U23VDDQSPI0HSIOPB8I/OAQSPI0_IO3I/O1PIO, I, PU, ST
BPCK3O1
DFLEXCOM2_IO1I/O2
V24VDDQSPI0HSIOPB9I/OAQSPI0_IO2I/O1PIO, I, PU, ST
DFLEXCOM2_IO0I/O2
EPWMEXTRG0I1
N21VDDQSPI0HSIOPB10I/OAQSPI0_IO1I/O1PIO, I, PU, ST
DFLEXCOM2_IO4O2
EPWMEXTRG1I1
U22VDDQSPI0HSIOPB11I/OAQSPI0_IO0I/O1PIO, I, PU, ST
DFLEXCOM2_IO5O2
EPWML3O1
FTIOB3I/O2
R20VDDQSPI0HSIOPB12I/OAQSPI0_CSO1PIO, I, PU, ST
DFLEXCOM2_IO3I/O2
EPWMFI1I1
FTIOA3I/O2
N20VDDQSPI0HSIOPB13I/OAQSPI0_SCKO1PIO, I, PU, ST
DFLEXCOM2_IO2I/O2
EPWMFI0I1
FTCLK3I2
R21VDDQSPI0HSIOPB14I/OAQSPI0_SCKNO1PIO, I, PU, ST
BQSPI1_SCKO1
CI2SMCC0_CKI/O3
DFLEXCOM10_IO5O1
EPWMH3O1
GFLEXCOM2_IO1I/O4
R22VDDQSPI0HSIOPB15I/OAQSPI0_IO4I/O1PIO, I, PU, ST
BQSPI1_IO0I/O1
CI2SMCC0_WSI/O3
DFLEXCOM10_IO6O1
EPWML0O1
FTCLK4I2
GFLEXCOM2_IO0I/O4
U24VDDQSPI0HSIOPB16I/OAQSPI0_IO5I/O1PIO, I, PU, ST
BQSPI1_IO1I/O1
CI2SMCC0_DIN0I3
DFLEXCOM10_IO4O1
EPWMH0O1
FTIOB4I/O2
M20VDDQSPI0HSIOPB17I/OAQSPI0_IO6I/O1PIO, I, PU, ST
BQSPI1_IO2I/O1
CI2SMCC0_DOUT0O3
DFLEXCOM10_IO3I/O1
EPWML1O1
FTIOA4I/O2
V25VDDQSPI0HSIOPB18I/OAQSPI0_IO7I/O1PIO, I, PU, ST
BQSPI1_IO3I/O1
CI2SMCC0_MCKO3
DFLEXCOM10_IO2I/O1
EPWMH1O1
FTIOA5I/O2
N22VDDQSPI0HSIOPB19I/OAQSPI0_DQSI1PIO, I, PU, ST
BEXT_IRQ1I2
CPCK4O1
DFLEXCOM10_IO1I/O1
EPWML2O1
FTIOB5I/O2
M19VDDQSPI0HSIOPB20I/OAQSPI0_INTI1PIO, I, PU, ST
BQSPI1_CSO1
DFLEXCOM10_IO0I/O1
EPWMH2O1
FTCLK5I2
F17VDDSDMMC1HSIOPB21I/OASDMMC1_RSTNO1PIO, I, PU, ST
BFLEXCOM6_IO4O2
CTIOB2I/O2
DADTRGI2
EEXT_IRQ0I2
A18VDDSDMMC1HSIOPB22I/OASDMMC1_CMDI/O1PIO, I, PU, ST
BFLEXCOM6_IO3I/O2
CTCLK2I2
D17VDDSDMMC1HSIOPB23I/OASDMMC1_CKO1PIO, I, PU, ST
BFLEXCOM6_IO2I/O2
CTIOA2I/O2
A17VDDSDMMC1HSIOPB24I/OASDMMC1_DAT0I/O1PIO, I, PU, ST
BFLEXCOM6_IO0I/O2
C17VDDSDMMC1HSIOPB25I/OASDMMC1_DAT1I/O1PIO, I, PU, ST
BFLEXCOM6_IO1I/O2
CTIOB2I/O1
B17VDDSDMMC1HSIOPB26I/OASDMMC1_DAT2I/O1PIO, I, PU, ST
BFLEXCOM8_IO0I/O3
CTCLK2I1
E17VDDSDMMC1HSIOPB27I/OASDMMC1_DAT3I/O1PIO, I, PU, ST
BFLEXCOM8_IO1I/O3
CTIOA2I/O1
A4VDDIN33GPIOPB28I/OAD12IASDMMC1_WPI1PIO, I, PU, ST
CFLEXCOM1_IO0I/O3
ED15I/O1,2
E11VDDIN33GPIOPB29I/OAD13IASDMMC1_CDI1PIO, I, PU, ST
BI2SMCC0_MCKO1
CFLEXCOM1_IO1I/O3
ED14I/O1,2
B5VDDIN33GPIOPB30I/OAD14IASDMMC1_1V8SELO1PIO, I, PU, ST
BI2SMCC1_MCKO1
CFLEXCOM1_IO2I/O3
DTIOA1I/O1
ENCS1/NANDCS1O1,2
B12VDDIN33GPIOPB31I/OHHSA_CC1I/OAPCK7O2PIO, I, PU, ST
BI2SMCC1_DIN1I1
CFLEXCOM1_IO3I/O3
DTCLK1I1
ENWE/NWR0/NANDWEO2
F15VDDIN33GPIOPC0I/OHHSA_CC2I/OAPCK6O2PIO, I, PU, ST
BI2SMCC1_DIN2I1
CFLEXCOM9_IO4O2
DTIOB1I/O1
ENWR1/NBS1O1,2
B11VDDIN33GPIOPC1I/OHHSB_CC1I/OAPCK5O1PIO, I, PU, ST
CFLEXCOM9_IO2I/O2
ESMCKO1,2
E15VDDIN33GPIOPC2I/OHHSB_CC2I/OAEXT_IRQ0I3PIO, I, PU, ST
CFLEXCOM9_IO3I/O2
EA11O1,2
F11VDDIN33GPIOPC3I/OAD0IASPDIF_RXI2PIO, I, PU, ST
CFLEXCOM9_IO0I/O2
DFLEXCOM0_IO4O2
EA10O1,2
A3VDDIN33GPIOPC4I/OAD1IASPDIF_TXO2PIO, I, PU, ST
CFLEXCOM9_IO1I/O2
DFLEXCOM0_IO3I/O2
ED0I/O2
G13VDDIN33GPIOPC5I/OAD2IAI3CC_SDASPUEO1PIO, I, PU, ST
BI2SMCC1_DIN3I1
DFLEXCOM0_IO2I/O2
ED1I/O2
J13VDDIN33GPIOPC6I/OAD3IAI3CC_SCLI/O1PIO, I, PU, ST
DFLEXCOM0_IO1I/O2
ED4I/O2
C9VDDIN33GPIOPC7I/OAD4I/OAI3CC_SDAI/O1PIO, I, PU, ST
DFLEXCOM0_IO0I/O2
ED5I/O2
D13VDDIN33GPIOPC8I/OACC_INP1IAI2SMCC0_DIN1I1PIO, I, PU, ST
BPDMC0_DS1I2
CI2SMCC1_DOUT1O1
DFLEXCOM9_IO0I/O1
ED6I/O2
B7VDDIN33GPIOPC9I/OACC_INN1IAI2SMCC0_DIN2I1PIO, I, PU, ST
BPDMC0_CLKO2
CI2SMCC1_DOUT2O1
DFLEXCOM9_IO1I/O1
ED7I/O2
H13VDDIN33GPIOPC10I/OAD5I/OAI2SMCC0_DIN3I1PIO, I, PU, ST
BPDMC0_DS0I2
CI2SMCC1_DOUT3O1
DFLEXCOM9_IO2I/O1
ED2I/O2
C5VDDIN33GPIOPC11I/OAD6IAI2SMCC0_DOUT1O1PIO, I, PU, ST
BPDMC1_DS0I1
DFLEXCOM9_IO3I/O1
ED3I/O2
H11VDDIN33GPIOPC12I/OAD7IAI2SMCC0_DOUT2O1PIO, I, PU, ST
BPDMC1_CLKO1
DFLEXCOM9_IO4O1
EA9O1,2
C7VDDIN33GPIOPC13I/OAD8IAI2SMCC0_DOUT3O1PIO, I, PD, ST
BPDMC1_DS1I1
EA8O1,2
J14VDDIN33GPIOPC14I/OAD9IAI2SMCC1_DIN0I1PIO, I, PD, ST
BSPDIF_RXI3
CFLEXCOM1_IO0I/O2
EA7O1,2
D7VDDIN33GPIOPC15I/OAD10IAI2SMCC1_WSI/O1PIO, I, PD, ST
BPDMC1_DS1I2
CFLEXCOM1_IO1I/O2
EA6O1,2
J11VDDIN33GPIOPC16I/OAD11IAI2SMCC1_CKI/O1PIO, I, PD, ST
BPDMC1_CLKO2
CFLEXCOM1_IO2I/O2
DTIOA1I/O2
EA5O1,2
A8VDDIN33GPIOPC17I/OACC_INP0IAI2SMCC1_DOUT0O1PIO, I, PU, ST
BPDMC1_DS0I2
CFLEXCOM1_IO3I/O2
DTCLK1I2
EA4O1,2
E13VDDIN33GPIOPC18I/OACC_INN2IAI2SMCC0_DIN0I1PIO, I, PU, ST
BSPDIF_TXO3
CFLEXCOM1_IO4O2
DTIOB1I/O2
EA3O1,2
A7VDDIN33GPIOPC19I/OACC_INP2IAI2SMCC0_WSI/O1PIO, I, PU, ST
BPCK6O1
EA2O1,2
A6VDDIN33GPIOPC20I/OACC_INN3AI2SMCC0_DOUT0O1PIO, I, PU, ST
EA1O1,2
G15VDDIN33GPIOPC21I/OACC_INP3AI2SMCC0_CKI/O1PIO, I, PU, ST
BPCK7O1
EA0/NBS0O1,2
D9VDDIN33GPIOPC22I/OAD15ANTRSTI1NTRST, PU, ST
ENWAITI1,2
A5VDDIN33GPIOPC23I/OATCK_SWCLKI1TCK_SWCLK, ST
D11VDDIN33GPIOPC24I/OATMS_SWDIOI/O1TMS_SWDIO, PU, ST
B6VDDIN33GPIOPC25I/OATDII1TDI, PU, ST
F13VDDIN33GPIOPC26I/OATDOO1TDO, ST
EA12O1,2
A19VDDSDMMC2HSIOPC27I/OASDMMC2_CMDI/O1PIO, I, PU, ST
BFLEXCOM8_IO0I/O2
DTD1O2
ED8I/O1,2
B19VDDSDMMC2HSIOPC28I/OASDMMC2_CKO1PIO, I, PU, ST
BFLEXCOM8_IO1I/O2
DTF1I/O2
ED9I/O1,2
A20VDDSDMMC2HSIOPC29I/OASDMMC2_DAT0I/O1PIO, I, PU, ST
BFLEXCOM8_IO2I/O2
DTK1I/O2
ED10I/O1,2
FTCLK0I1
C19VDDSDMMC2HSIOPC30I/OASDMMC2_DAT1I/O1PIO, I, PU, ST
BFLEXCOM8_IO3I/O2
DRD1I2
ED11I/O1,2
FTIOA0I/O1
B20VDDSDMMC2HSIOPC31I/OASDMMC2_DAT2I/O1PIO, I, PU, ST
BFLEXCOM8_IO4O2
CPCK0O2
DRK1I/O2
ED12I/O1,2
FTIOB0I/O1
D20VDDSDMMC2HSIOPD0I/OASDMMC2_DAT3I/O1PIO, I, PU, ST
CPCK1O2
DRF1I/O2
ED13I/O1,2
A21VDDIOP1GPIOPD1I/OASDMMC2_WPI1PIO, I, PU, ST
BFLEXCOM1_IO5O1
CLCDC_HSYNCO2
DFLEXCOM3_IO0I/O3
D19VDDIOP1GPIOPD2I/OASDMMC2_CDI1PIO, I, PU, ST
BFLEXCOM1_IO6O1
CLCDC_VSYNCO2
DFLEXCOM3_IO1I/O3
B21VDDIOP1GPIOPD3I/OASDMMC2_1V8SELO1PIO, I, PU, ST
BFLEXCOM1_IO4O1
CTIOA0I/O2
DFLEXCOM3_IO2I/O3
EEXT_IRQ1I3
G20VDDIOP1GPIOPD4I/OALCDC_HSYNCO1PIO, I, PU, ST
BFLEXCOM1_IO2I/O1
CTIOB0I/O2
DFLEXCOM7_IO1I/O3
C21VDDIOP1GPIOPD5I/OALCDC_VSYNCO1PIO, I, PU, ST
BFLEXCOM1_IO3I/O1
CTCLK0I2
DFLEXCOM7_IO0I/O3
E21VDDIOP1GPIOPD6I/OALCDC_PWMO1,2PIO, I, PU, ST
BFLEXCOM1_IO1I/O1
DFLEXCOM7_IO2I/O3
B22VDDIOP1GPIOPD7I/OALCDC_DISPO1,2PIO, I, PU, ST
BFLEXCOM1_IO0I/O1
DFLEXCOM7_IO3I/O3
G21VDDIOP1GPIOPD8I/OACANTX0O1PIO, I, PU, ST
BFLEXCOM7_IO0I/O1
A22VDDIOP1GPIOPD9I/OACANRX0I1PIO, I, PU, ST
BFLEXCOM7_IO1I/O1
E22VDDIOP1GPIOPD10I/OACANTX1O1PIO, I, PU, ST
BFLEXCOM7_IO2I/O1
CTIOA1I/O3
A23VDDIOP1GPIOPD11I/OACANRX1I1PIO, I, PU, ST
BFLEXCOM7_IO3I/O1
CTCLK1I3
B25VDDIOP1GPIOPD12I/OACANTX2O1PIO, I, PU, ST
BFLEXCOM7_IO4O1
CTIOB1I/O3
DPCK2O2
EFLEXCOM3_IO3I/O3
C23VDDIOP1GPIOPD13I/OACANRX2I1PIO, I, PU, ST
BFLEXCOM5_IO4O1
CTIOA2I/O3
DPCK3O2
C25VDDIOP1GPIOPD14I/OACANTX3O1PIO, I, PU, ST
BFLEXCOM5_IO2I/O1
CTIOB2I/O3
C24VDDIOP1GPIOPD15I/OACANRX3I1PIO, I, PU, ST
BFLEXCOM5_IO3I/O1
CTCLK2I3
D25VDDIOP1GPIOPD16I/OACANTX4O1PIO, I, PU, ST
BFLEXCOM5_IO0I/O1
E23VDDIOP1GPIOPD17I/OACANRX4I1PIO, I, PU, ST
BFLEXCOM5_IO1I/O1
G22VDDGMAC1GPIOPD18I/OBFLEXCOM6_IO0I/O4PIO, I, PU, ST
CCANTX1O2
DPCK4O2
E24VDDGMAC1GPIOPD19I/OBFLEXCOM6_IO1I/O4PIO, I, PU, ST
CCANRX1I2
DPCK2O3
J18VDDGMAC1GPIOPD20I/OBFLEXCOM6_IO2I/O4PIO, I, PU, ST
CI2SMCC1_MCKO2
DPCK3O3
K19VDDGMAC1GPIOPD21I/OAG1_TXCTL/G1_TXENO1,2PIO, I, PU, ST
BFLEXCOM6_IO2I/O3
CTK1I/O1
E25VDDGMAC1GPIOPD22I/OAG1_TX0O1,2PIO, I, PU, ST
BFLEXCOM6_IO3I/O3,4
CTF1I/O1
G23VDDGMAC1GPIOPD23I/OAG1_TX1O1,2PIO, I, PU, ST
BFLEXCOM6_IO4O3,4
CTD1O1
F25VDDGMAC1GPIOPD24I/OAG1_RXCTL/G1_CRSDVI1,2PIO, I, PU, ST
BFLEXCOM6_IO0I/O3
CRD1I1
EPDMC0_DS1I3
J20VDDGMAC1GPIOPD25I/OAG1_MDCO1,2PIO, I, PU, ST
BFLEXCOM6_IO1I/O3
CRK1I/O1
EPDMC0_CLKO3
G25VDDGMAC1GPIOPD26I/OAG1_MDIOI/O1,2PIO, I, PU, ST
BFLEXCOM7_IO4O2
CRF1I/O1
DI2SMCC1_DIN2I2
EPDMC0_DS0I3
J21VDDGMAC1GPIOPD27I/OAG1_RX0I1,2PIO, I, PU, ST
BFLEXCOM7_IO0I/O2
CSPDIF_RXI1
DI2SMCC1_DIN3I2
G24VDDGMAC1GPIOPD28I/OAG1_RX1I1,2PIO, I, PU, ST
BFLEXCOM7_IO1I/O2
CSPDIF_TXO1
DI2SMCC1_DIN1I2
J24VDDGMAC1GPIOPD29I/OAG1_REFCK/G1_TXCKI/O2,1PIO, I, PU, ST
BFLEXCOM7_IO2I/O2
CI2SMCC1_DOUT3O2
H25VDDGMAC1GPIOPD30I/OAG1_RX2I1PIO, I, PU, ST
BFLEXCOM7_IO3I/O2
CI2SMCC1_DOUT1O2
DPDMC1_DS1I3
EG1_RXERI2
J25VDDGMAC1GPIOPD31I/OAG1_RX3I1PIO, I, PU, ST
BFLEXCOM5_IO4O2
CI2SMCC1_DOUT2O2
DPDMC1_DS0I3
J23VDDGMAC1GPIOPE0I/OAG1_TX2O1PIO, I, PU, ST
BFLEXCOM5_IO2I/O2
CI2SMCC1_DIN0I2
DPDMC1_CLKO3
K25VDDGMAC1GPIOPE1I/OAG1_TX3O1PIO, I, PU, ST
BFLEXCOM5_IO3I/O2
CI2SMCC1_WSI/O2
DPDMC0_DS1I4
J22VDDGMAC1GPIOPE2I/OAG1_RXCKI1PIO, I, PU, ST
BFLEXCOM5_IO1I/O2
CI2SMCC1_CKI/O2
DPDMC0_CLKO4
L25VDDGMAC1GPIOPE3I/OAG1_TSUCOMPO1,2PIO, I, PU, ST
BFLEXCOM5_IO0I/O2
CI2SMCC1_DOUT0O2
DPDMC0_DS0I4
Y11VDDLVDSGPIOPE4I/OLVDS_A0MOALCDC_DAT0O1,2PIO, I, PU, ST
BFLEXCOM2_IO2I/O1
CPWML0O2
DTIOA3I/O1
EI2SMCC0_DIN1I2
AA11VDDLVDSGPIOPE5I/OLVDS_A0POALCDC_DAT1O1,2PIO, I, PU, ST
BFLEXCOM2_IO3I/O1
CPWMH0O2
DTIOB3I/O1
EI2SMCC0_DIN2I2
Y12VDDLVDSGPIOPE6I/OLVDS_A1MOALCDC_DAT2O1,2PIO, I, PU, ST
BFLEXCOM2_IO4O1
CPWML1O2
DTCLK3I1
EI2SMCC0_DIN3I2
AA12VDDLVDSGPIOPE7I/OLVDS_A1POALCDC_DAT3O1,2PIO, I, PU, ST
BFLEXCOM2_IO5O1
CPWMH1O2
DTIOA4I/O1
EI2SMCC0_DOUT1O2
Y13VDDLVDSGPIOPE8I/OLVDS_A2MOALCDC_DAT4O1,2PIO, I, PU, ST
BFLEXCOM2_IO0I/O1
CPWML2O2
DTIOB4I/O1
EI2SMCC0_CKI/O2
AA13VDDLVDSGPIOPE9I/OLVDS_A2POALCDC_DAT5O1,2PIO, I, PU, ST
BFLEXCOM2_IO1I/O1
CPWMH2O2
DTCLK4I1
EI2SMCC0_WSI/O2
Y15VDDLVDSGPIOPE10I/OLVDS_A3MOALCDC_DAT6O1,2PIO, I, PU, ST
BFLEXCOM2_IO6O1
CPWML3O2
DTIOA5I/O1
EI2SMCC0_DOUT2O2
AA15VDDLVDSGPIOPE11I/OLVDS_A3POALCDC_DAT7O1,2PIO, I, PU, ST
CPWMH3O2
DTIOB5I/O1
EI2SMCC0_DOUT3O2
Y14VDDLVDSGPIOPE12I/OLVDS_CLK1MOALCDC_DENO1,2PIO, I, PU, ST
BPCK3O4
CPWMEXTRG0I2
DTCLK5I1
EI2SMCC0_DIN0I2
AA14VDDLVDSGPIOPE13I/OLVDS_CLK1POALCDC_PCKO1,2PIO, I, PU, ST
BPCK4O3
CPWMEXTRG1I2
EI2SMCC0_DOUT0O2
B4VDDIN33Analog inputADVREFPI
F14VDDIN33powerVDDIN33I
H16GNDIN33groundGNDIN33I
F16GNDANAgroundGNDANAI
E10GNDANAgroundGNDANAI
E12GNDANAgroundGNDANAI
N16GNDANAgroundGNDANAI
Y18VDDIOP0powerVDDIOP0I
K24VDDGMAC0powerVDDGMAC0I
F21VDDIOP1powerVDDIOP1I
F24VDDGMAC1powerVDDGMAC1I
A1GNDgroundGNDI
A25GNDgroundGNDI
AA1GNDgroundGNDI
AA4GNDgroundGNDI
AA6GNDgroundGNDI
D4GNDgroundGNDI
D24GNDgroundGNDI
E2GNDgroundGNDI
E5GNDgroundGNDI
E8GNDgroundGNDI
E14GNDgroundGNDI
E18GNDgroundGNDI
E16VDDANApowerVDDANAI
F10VDDANApowerVDDANAI
F12VDDANApowerVDDOUT25O
V15VDDANApowerVDDIN25I
L1GNDgroundGND
G11VDDCOREpowerVDDCOREI
N19VDDCOREpowerVDDCOREI
H12VDDCOREpowerVDDCOREI
F1GNDgroundGNDI
K17VDDCOREpowerVDDCOREI
K20VDDCOREpowerVDDCOREI
L13VDDCOREpowerVDDCOREI
M12VDDCOREpowerVDDCOREI
N17VDDCOREpowerVDDCOREI
V19VDDCOREpowerVDDCOREI
P21VDDCOREpowerVDDCOREI
T14VDDCOREpowerVDDCOREI
T24VDDCOREpowerVDDCOREI
Y16VDDCOREpowerVDDCOREI
G19VDDCPUpowerVDDCPUI
H20VDDCPUpowerVDDCPUI
H24VDDCPUpowerVDDCPUI
J19VDDCPUpowerVDDCPUI
K18VDDCPUpowerVDDCPUI
J17VDDCOREpowerVDDCOREI
F9GNDgroundGNDI
F20GNDgroundGNDI
G2GNDgroundGNDI
G3GNDgroundGNDI
G5GNDgroundGNDI
G7GNDgroundGNDI
G9GNDgroundGNDI
H1GNDgroundGNDI
H5GNDgroundGNDI
H8GNDgroundGNDI
H10GNDgroundGNDI
H18GNDgroundGNDI
H21GNDgroundGNDI
J1GNDgroundGNDI
J3GNDgroundGNDI
J5GNDgroundGNDI
J7GNDgroundGNDI
P16GNDgroundGNDI
T16VDDLVDSpowerVDDLVDSI
H14GNDUTMIgroundGNDUTMII
J15VDDUTMIpowerVDDUTMII
B1VDDUTMIHHSDPAI/O
B2VDDUTMIHHSDMAI/O
C1VDDUTMIHHSDPBI/O
C2VDDUTMIHHSDMBI/O
D1VDDUTMIHHSDPCI/O
D2VDDUTMIHHSDMCI/O
C3VDDUTMIAnalog inputHHSRTUNEI
K12VDDIODDRpowerVDDIODDRI
K14VDDIODDRpowerVDDIODDRI
L9VDDIODDRpowerVDDIODDRI
L10VDDIODDRpowerVDDIODDRI
L11VDDIODDRpowerVDDIODDRI
L15VDDIODDRpowerVDDIODDRI
M9VDDIODDRpowerVDDIODDRI
M10VDDIODDRpowerVDDIODDRI
M14VDDIODDRpowerVDDIODDRI
M16VDDIODDRpowerVDDIODDRI
N11VDDIODDRpowerVDDIODDRI
N13VDDIODDRpowerVDDIODDRI
N15VDDIODDRpowerVDDIODDRI
P10VDDIODDRpowerVDDIODDRI
P12VDDIODDRpowerVDDIODDRI
J9GNDgroundGNDI
J10GNDgroundGNDI
K2GNDgroundGNDI
K8GNDgroundGNDI
K10GNDgroundGNDI
K11GNDgroundGNDI
K13GNDgroundGNDI
K15GNDgroundGNDI
K21GNDgroundGNDI
AA8GNDgroundGNDI
AA10GNDgroundGNDI
AA25GNDgroundGNDI
B16GNDgroundGNDI
B24GNDgroundGNDI
E4VDDIODDRAnalog inputDDR_VREFI
J12VDDIODDRAnalog inputDDR_ZQO
P20VDDDPHYpowerVDDDPHYI
M21GNDDPHYgroundGNDDPHYI
Y22VDDDPHYMIPI_CLKNO
AA22VDDDPHYMIPI_CLKPO
Y20VDDDPHYMIPI_DN0O
AA20VDDDPHYMIPI_DP0O
Y21VDDDPHYMIPI_DN1O
AA21VDDDPHYMIPI_DP1O
Y24VDDDPHYMIPI_DN2O
Y25VDDDPHYMIPI_DP2O
W24VDDDPHYMIPI_DN3O
W25VDDDPHYMIPI_DP3O
AA23VDDDPHYMIPI_REXTI
U21VDDSDMMC0powerVDDSDMMC0I
B18VDDSDMMC1powerVDDSDMMC1I
T20VDDSDMMC0Analog inputSDMMC0_CALI
F18VDDSDMMC1Analog inputSDMMC1_CALI
D22VDDSDMMC2powerVDDSDMMC2I
E19VDDSDMMC2Analog inputSDMMC2_CALI
J16GNDBATgroundGNDBATI
K16VBATpowerVBATI
G17VBATPIOBUPIOBU0IPU(5)
B14VBATPIOBUPIOBU1IPU(5)
C15VBATPIOBUPIOBU2IPU(5)
A13VBATPIOBUPIOBU3IPD(5)
B10VDDIN33XINI
A10VDDIN33XOUTO
A15VBATXIN32I
B15VBATXOUT32O
D15VBATTSTIPD
C13VBATJTAGSELIPD
A16VBATWKUP0I
B13VBATSHDNO
B9VDDIN33NRSTIPU
B8VDDIN33NRST_OUTOOD(6)
C11VDDIN33GPIOAUDIOCLKO
A12VBATbackup I/OLPMO
M24VDDQSPI0powerVDDQSPI0I
L22VDDQSPI0Analog inputQSPI0_CALI
A14GNDgroundGNDI
H15GNDgroundGNDI
A11GNDgroundGNDI
A9GNDgroundGNDI
AA3DDRM_VDDpowerDDRM_VDDI
AA5DDRM_VDDpowerDDRM_VDDI
AA7DDRM_VDDpowerDDRM_VDDI
AA9DDRM_VDDpowerDDRM_VDDI
E1DDRM_VDDpowerDDRM_VDDI
E3DDRM_VDDpowerDDRM_VDDI
E7DDRM_VDDpowerDDRM_VDDI
E9DDRM_VDDpowerDDRM_VDDI
F2DDRM_VDDpowerDDRM_VDDI
F5DDRM_VDDpowerDDRM_VDDI
F6DDRM_VDDpowerDDRM_VDDI
F8DDRM_VDDpowerDDRM_VDDI
G1DDRM_VDDpowerDDRM_VDDI
G4DDRM_ZQAnalog inputDDRM_ZQI
G6DDRM_VDDpowerDDRM_VDDI
H2DDRM_VDDpowerDDRM_VDDI
H6DDRM_VDDpowerDDRM_VDDI
J2DDRM_VDDpowerDDRM_VDDI
J4DDRM_VDDpowerDDRM_VDDI
J6DDRM_VDDpowerDDRM_VDDI
K1DDRM_VDDpowerDDRM_VDDI
K5DDRM_VDDpowerDDRM_VDDI
K6DDRM_VDDpowerDDRM_VDDI
K7DDRM_VDDpowerDDRM_VDDI
K9DDRM_VDDpowerDDRM_VDDI
L2DDRM_VDDpowerDDRM_VDDI
L3GNDgroundGNDI
L4DDRM_VDDpowerDDRM_VDDI
L5GNDgroundGNDI
L6DDRM_VDDpowerDDRM_VDDI
L7GNDgroundGNDI
L8GNDgroundGNDI
L12GNDgroundGNDI
L14GNDgroundGNDI
L16GNDgroundGNDI
L17GNDgroundGNDI
L18GNDgroundGNDI
M1DDRM_VDDpowerDDRM_VDDI
M2GNDgroundGNDI
M5GNDgroundGNDI
M6GNDgroundGNDI
M7DDRM_VDDpowerDDRM_VDDI
M8GNDgroundGNDI
M11GNDgroundGNDI
M13GNDgroundGNDI
M15GNDgroundGNDI
M17GNDgroundGNDI
M18GNDgroundGNDI
N1GNDgroundGNDI
N2GNDgroundGNDI
N3DDRM_VDDpowerDDRM_VDDI
N4GNDgroundGNDI
N5DDRM_VDDpowerDDRM_VDDI
N6DDRM_VDDpowerDDRM_VDDI
N7GNDgroundGNDI
N8DDRM_VDDpowerDDRM_VDDI
N9GNDgroundGNDI
N10GNDgroundGNDI
N12GNDgroundGNDI
N14GNDgroundGNDI
N18GNDgroundGNDI
P1DDRM_VDDpowerDDRM_VDDI
P2GNDgroundGNDI
P5GNDgroundGNDI
P6DDRM_VDDpowerDDRM_VDDI
P8GNDgroundGNDI
P11GNDgroundGNDI
P13GNDgroundGNDI
P14VDDIODDRpowerVDDIODDRI
P18GNDgroundGNDI
P24GNDgroundGNDI
R1GNDgroundGNDI
R2DDRM_VDDpowerDDRM_VDDI
R3GNDgroundGNDI
R4DDRM_VDDpowerDDRM_VDDI
R5DDRM_VDDpowerDDRM_VDDI
R6GNDgroundGNDI
R7GNDgroundGNDI
R9DDRM_VDDpowerDDRM_VDDI
R10GNDgroundGNDI
R11GNDgroundGNDI
R12DDR_VREFAnalog inputDDR_VREFI
R13VDDIODDRpowerVDDIODDRI
R19GNDgroundGNDI
T1DDRM_VDDpowerDDRM_VDDI
T2GNDgroundGNDI
T5GNDgroundGNDI
T6DDRM_VDDpowerDDRM_VDDI
T8DDRM_VDDpowerDDRM_VDDI
T9GNDgroundGNDI
T10DDRM_VDDpowerDDRM_VDDI
T11GNDgroundGNDI
T12GNDgroundGNDI
T15GNDgroundGNDI
T21GNDgroundGNDI
U1GNDgroundGNDI
U2DDRM_VDDpowerDDRM_VDDI
U3GNDgroundGNDI
U4DDRM_VDDpowerDDRM_VDDI
U5DDRM_VDDpowerDDRM_VDDI
U7DDRM_VDDpowerDDRM_VDDI
U8GNDgroundGNDI
U9DDRM_VDDpowerDDRM_VDDI
U10GNDgroundGNDI
U12GNDgroundGNDI
U14GNDgroundGNDI
U16GNDgroundGNDI
U18GNDgroundGNDI
V1DDRM_VDDpowerDDRM_VDDI
V2GNDgroundGNDI
V4GNDgroundGNDI
V6DDRM_VDDpowerDDRM_VDDI
V7GNDgroundGNDI
V9GNDgroundGNDI
V20GNDgroundGNDI
V22GNDgroundGNDI
W1GNDgroundGNDI
W2DDRM_VDDpowerDDRM_VDDI
W3GNDgroundGNDI
W5GNDgroundGNDI
W6DDRM_VDDpowerDDRM_VDDI
W7DDRM_VDDpowerDDRM_VDDI
W9DDRM_VDDpowerDDRM_VDDI
W11GNDgroundGNDI
W15GNDgroundGNDI
W23GNDgroundGNDI
Y1DDRM_VDDpowerDDRM_VDDI
Y2GNDgroundGNDI
Y4DDRM_VDDpowerDDRM_VDDI
Y5GNDgroundGNDI
Y6DDRM_VDDpowerDDRM_VDDI
Y7GNDgroundGNDI
Y8DDRM_VDDpowerDDRM_VDDI
Y9GNDgroundGNDI
Y10DDRM_VDDpowerDDRM_VDDI
Note:
  1. I/Os for each peripheral are grouped into I/O sets, listed in the column "I/O Set". For all peripherals, use I/Os that belong to the same I/O set. Timings can be unpredictable when I/Os from different I/O sets are mixed.
  2. When using an I/O line with the Analog-to-Digital Converter (ADC) or with the Analog Comparator Controller (ACC), the PIO line configuration (pull-up, pull-down) programmed before assigning this line to the ADC or ACC peripheral is not modified by this peripheral.
  3. Refer to I/O Characteristics in the Electrical Characteristics section of the SAMA7D6 Series data sheet for the definition of I/Os.
  4. PU=Pull-Up, PD=Pull-Down, HiZ=High Impedance, ST=Schmitt Trigger
  5. This is the PIOBU state after VBAT power-up. If programmed to another value, this value is maintained as long as VBAT is not removed.
  6. Open-drain output requires an external resistor.