6.2.6.2 ACTIVATE [off | url URL | isv ISVNAME]

The ACTIVATE line allows you to disable the “Activate License” command, or to set the defaults for the URL and ISV name for activation.

The three forms of the ACTIVATE line are:

  • ACTIVATE off
  • ACTIVATE url URL
  • ACTIVATE url ISVNAME

In the first form, the “Activate License” menu item is disabled and will not appear in the menus. In the second form “URL” is the default URL used for activation. For example:

ACTIVATE url www.reprisesoftware.com

In the third form “ISVNAME” is the default ISV name used for activation. For example:

ACTIVATE isv reprise