Changes reflect that the RLM License
Administration Manual has been updated to v14.1 on September 2020.
Chapter 1. “Network License Server Overview”: Updated content as virtual
machines now supported and the server need not be running a server-grade OS. Figure
1.1 “Network License Client/Server Model” has been updated for one or more installed
licenses and Table 1-2 “License Server Software Platforms” has been updated for
64-bit only operation. A security note has been added to state that the server
should not be exposed to the public internet .
Chapter 2. “Network License Server Installation”: All screen images
updated.
Chapter 3. “Network License Server
Startup”: Example 3-1 updated. Section 3.1 “Installing License Server on a
Virtual Machine” has been added. Section 3.4 “Running the License Server as a
Service” updated with the latest RLM manual content.
Chapter 4. “Considerations for Running MPLAB XC License Server on Cloud
Platforms”: New chapter.
Chapter 5. “How To’s”: Under
Section 5.1 “Change the default ports that are used”, Figure 5-1 “Compiler
Installation - Network Client” has been updated. Sections 5.6 through 5.8 show the
updated server install directory.
Chapter 6. “RLM End User Manual - Extracts” (Previously Appendix A): Extracts
based on the updated v14.1 manual. Changes of note are:
Section 6.1 “RLM End User Manual Versions”: New section added.
Section 6.2.1 “The License
Server”: Added Note that you should NEVER run the rlm servers as a
privileged user. In Section 6.2.1.1 “rlm startup options”, added
-iai, -user username and
-password password. In Section 6.2.1.2 “License Server
Startup Processing”, provide link to how to run server on a virtual
machine.
Section 6.2.2.5.1.2 “Optional Parameters”: The table under
platforms=platform-list must be updated for 64-bit only
operation.
Section 6.2.3 “License Administration Tools”: Added Section 6.2.3.1
“rlmadduser – add a user to the ISV server options file”. In Sections
6.2.3.4 “rlmdown - shuts down the license server” and 6.2.3.9 “rlmstat -
obtains status from the license servers”, added [-c
license_file] option. In Section 6.2.3.5 “rlmhostid - print the
hostid of this machine”, new options added.
Section 6.2.4 “Client Authentication”: New section added.
Section 6.2.5 “The RLM Web Server”: New note that web server is disabled if
the user running rlm is root or an admin user. In Section 6.2.5.1 “Access
Control to the RLM Web Interface”, extend_roam added to
Table 6-3 “RLM privileges assignable in the RLM password file”. Sections
6.2.5.2 “Intro Screen” and 6.2.5.5 “License Status” have updated
graphics.
Section 6.2.7.19 “PURGE_REPORTLOG #days” added.
Sections 6.3.1 “How to Queue for Licenses” and 6.3.2.2 “How to make a
License Roam”: Added a note about setting RLM_ROAM causes setting RLM_QUEUE
to be ignored .
Section 6.3.3 (A.10) “Failover License Servers” has been removed.
Section 6.4.2 :Reportlog File Format”: In Section 6.4.2.1 “Authentication
data”, added BADAUTH. In Section 6.4.2.2 “checkin”, why value of 11
added to table. In Section 6.4.2.3 “checkout”, added statement about
client-ip-address. Section 6.4.2.5 “dynamic
reservation” added new. In Section 6.4.2.9 “log file start”, SWITCH and
TIMEZONE added.