7.2.10 Function acc_set_input()

Set the ACC comparator plus/minus input sources.

void acc_set_input( Acc * p_acc, uint32_t ul_select_minus, uint32_t ul_select_plus)

Table 7-12. Parameters
Data directionParameter nameDescription

[in, out]

p_acc

Module hardware register base address pointer

[in]

ul_select_minus

Selection for the minus comparator input (inn)

[in]

ul_select_plus

Selection for the plus comparator input (inp)

Where the input parameter ul_select_minus is one of the following:

Parameter Value

Description

ACC_MR_SELMINUS_TS

Select TS as the minus input

ACC_MR_SELMINUS_ADVREF

Select ADVREF as the minus input

ACC_MR_SELMINUS_DAC0

Select DAC0 as the minus input

ACC_MR_SELMINUS_DAC1

Select DAC1 as the minus input

ACC_MR_SELMINUS_AD0

Select AD0 as the minus input

ACC_MR_SELMINUS_AD1

Select AD1 as the minus input

ACC_MR_SELMINUS_AD2

Select AD2 as the minus input

ACC_MR_SELMINUS_AD3

Select AD3 as the minus input

Where the input parameter ul_select_plus is one of the following:

Parameter Value

Description

ACC_MR_SELPLUS_AD0

Select AD0 as the plus input

ACC_MR_SELPLUS_AD1

Select AD1 as the plus input

ACC_MR_SELPLUS_AD2

Select AD2 as the plus input

ACC_MR_SELPLUS_AD3

Select AD3 as the plus input

ACC_MR_SELPLUS_AD4

Select AD4 as the plus input

ACC_MR_SELPLUS_AD5

Select AD5 as the plus input

ACC_MR_SELPLUS_AD6

Select AD6 as the plus input

ACC_MR_SELPLUS_AD7

Select AD7 as the plus input