21.9 Frame transmitted despite confirmed transmit cancellation for CAN-FD messages with more than 8 data bytes

Attention: This erratum is not relevant for CAN 2.0.

In case the transmission of Tx Buffer nn was not successful and is restarted immediately afterwards by automatic retransmission, and the software requests a Tx cancellation for this Tx Buffer by setting the cancellation request bit MCAN_TXBCR.CRnn during transmission of the first 4 identifier bits, a successful cancellation is incorrectly signalled by setting MCAN_TXBCF.CFnn = ’1’ and by clearing MCAN_TXBRP.TRPnn. In addition, the respective Transmission Occurred bit remains zero (MCAN_TXBTO.TOnn = ’0’), incorrectly indicating that the frame was not transmitted on the bus.

Other than signalled by MCAN_TXBCF.CFnn and MCAN_TXBTO.TOnn, the transmission continues until the complete frame has been sent on the CAN bus. If the transmission is successful, MCAN_TXBTO.TOnn will be set.

If in this case new data is written to Tx Buffer nn while the transmission is still ongoing, a frame with inconsistent data may appear on the bus.

This problem is limited to the case of transmit cancellation of CAN-FD messages with more than 8 data bytes while automatic retransmission is enabled (MCAN_CCCR.DAR = ’0’).

Transmit cancellation of Classical CAN messages and CAN-FD messages with up to 8 data bytes is not affected.

CAN 2.0 operation is not impacted.

Work Around

Do not use transmit cancellation for CAN-FD messages with more than 8 data bytes.

Alternatively, wait for the duration of the expected transmission time of the cancelled Tx Buffer before writing new data to that Tx Buffer.

Affected Silicon Revisions

A0A1A1-D1GA1-D2G
XXXX