21.1 Edge filtering causes mis-synchronization when falling edge at Rx input pin coincides with end of integration phase
When edge filtering is enabled (MCAN_CCCR.EFBI = ’1’) and when the end of the integration phase coincides with a falling edge at the Rx input pin, it may happen that the MCAN synchronizes itself wrongly and does not correctly receive the first bit of the frame. In this case the CRC will detect that the first bit was received incorrectly; it will rate the received FD frame as faulty and an error frame will be sent.
The issue only occurs when there is a falling edge at the Rx input pin (CANRX) within the last time quantum (tq) before the end of the integration phase. The last time quantum of the integration phase is at the sample point of the 11th recessive bit of the integration phase. When the edge filtering is enabled, the bit timing logic of the MCAN sees the Rx input signal delayed by the edge filtering. When the integration phase ends, the edge filtering is automatically disabled. This affects the reset of the FD CRC registers at the beginning of the frame. The Classical CRC registers are not affected, so this issue does not affect the reception of Classical frames.
In CAN communication, the MCAN may enter integrating state (either by resetting MCAN_CCCR.INIT or by protocol exception event) while a frame is active on the bus. In this case the 11 recessive bits are counted between the Acknowledge bit and the following start of frame. All nodes have synchronized at the beginning of the dominant Acknowledge bit. This means that the edge of the following Start-of-Frame bit cannot fall on the sample point, so the issue does not occur. The issue occurs only when the MCAN is, by local errors, mis-synchronized with regard to the other nodes, or not synchronized at all.
Glitch filtering as specified in ISO 11898-1:2015 is fully functional.
Edge filtering was introduced for applications where the data bit time is at least two tq (of the nominal bit time) long. In that case, edge filtering requires at least two consecutive dominant time quanta before the counter counting the 11 recessive bits for idle detection is restarted. This means edge filtering covers the theoretical case of occasional 1-tq-long dominant spikes on the CAN bus that would delay idle detection. Repeated dominant spikes on the CAN bus would disturb all CAN communication, so the filtering to speed up idle detection would not help network performance.
When this rare event occurs, the MCAN sends an error frame and the sender of the affected frame retransmits the frame. When the retransmitted frame is received, the MCAN has left the integration phase and the frame will be received correctly. Edge filtering is only applied during integration phase; it is never used during normal operation. As the integration phase is very short with respect to “active communication time”, the impact on total error frame rate is negligible. The issue has no impact on data integrity.
- when MCAN_CCCR.INIT is set to ’0’ after start-up
- after a protocol exception event (only when MCAN_CCCR.PXHD = ’0’)
Work Around
Disable edge filtering or wait on retransmission in case this rare event happens.
Affected Device Revisions
| A0 | A1 | A1-D1G | A1-D2G | A1-D4G | |||
| X | X | X | X | X |