21.4 Tx FIFO message sequence inversion
- Position 1: Tx FIFO message 1 (transmission ongoing)
- Position 2: Tx FIFO message 2
- Position 3: --
- Position 1: Tx FIFO message 1 (transmission ongoing)
- Position 2: non-Tx FIFO message with higher CAN priority
- Position 3: Tx FIFO message 2
- Position 1: non-Tx FIFO message with higher CAN priority (transmission ongoing)
- Position 2: Tx FIFO message 2
- Position 3: Tx FIFO message 1
Now Tx FIFO message 2 is in the output pipeline in front of Tx FIFO message 1 and they are transmitted in that order, resulting in a message sequence inversion.
Work Around
1. First Work Around
Use two dedicated Tx Buffers, e.g. use Tx Buffers 4 and 5 instead of the Tx FIFO. The pseudo-code below replaces the function that fills the Tx FIFO.
Write message to Tx Buffer 4.
- Request Tx Buffer 4 - write MCAN_TXBAR.A4
- Write message to Tx Buffer 5
- Wait until transmission of Tx Buffer 4 completed - MCAN_IR.TC, read MCAN_TXBTO.TO4
- Request Tx Buffer 5 - write MCAN_TXBAR.A5
- Write message to Tx Buffer 4
- Wait until transmission of Tx Buffer 5 is completed - MCAN_IR.TC, read MCAN_TXBTO.TO5
2. Second Work Around
Make sure that only one Tx FIFO element is pending for transmission at any time. The Tx FIFO elements may be filled at any time with messages to be transmitted, but their transmission requests are handled separately. Each time a Tx FIFO transmission has completed and the Tx FIFO gets empty (MCAN_IR.TFE = ’1’), the next Tx FIFO element is requested.
3. Third Work Around
Use only a Tx FIFO. Send the message with the higher priority also from Tx FIFO.
One drawback is that the higher priority message has to wait until the preceding messages in the Tx FIFO have been sent.
Affected Device Revisions
| A0 | A1 | A1-D1G | A1-D2G | A1-D4G | |||
| X | X | X | X | X |