37.9 Effects of Reset
Following any Reset event, all the ADC control and status registers are reset to their default
values with control bits in a non-active state. This disables the ADC cores and sets the analog input pins to Analog Input mode. Any conversion that was in
progress terminates, and the result cannot be written to the result buffer. The values in the
ADCDATAx registers are initialized to 0x00000000 during a device Reset. The
bias circuits are also turned OFF, so the ADC resuming operations wait for the bias circuits
to stabilize by polling (or requesting to be interrupted by) the BGVRRDY bit (ADCCON2
register).