17.9 Intellectual Property Protection
Intellectual property protection consists of restricting access to internal memories from external tools when the device is protected, and the user can accomplish this by setting the Code Protect bit or DEBUG_LCK bit.
- Code Protect – If enabling the Code Protect bit
by configuring FCPN0.CP in Boot Flash memory, the device is locked from programming and
debugging. Only chip erase can retrieve the device to the normal programming and debugging condition.Note:
- It is not possible to enter Debug Mode when Code Protect is active.
- Programming the Flash is only possible when the device is not code protected.
- If the device is already code protected, issue chip erase procedure to make the device un-protected and programming ready.
- Issue the Chip-Erase command by writing a ‘
1’ to DSU.CTRL.CE. The device then:- Clears the system volatile memories only when code protect is enabled.
- Erases the whole Flash array (excluding OTP, TCFG).
- Secured Device – DEBUG_LCK bits in eFuse (SECCFG.DEBUG_LCK in Root of Trust) determines if the device is locked for debugging. If the DEBUG_LCK bits are non-zero, device is a secured device. Securing of the device implies:
- The user cannot execute any unauthenticated firmware.
- The debug features of the device are not available and are locked down.
- Device programming through SWD interface is still available. Debugger can be plugged in only through the Cold-Plugging procedure. The Hot-Plugging feature is not available (see Cold-Plugging and Hot-Plugging from Related Links).
- The DEBUG_LCK bits are in eFuse (one time programmable memory); therefore, when locked, the device is permanently locked for debug unlike the Code Protect mechanism, which can be cleared on a chip erase.
When the device is protected, read/write accesses using the AHB-AP is limited to the DSU address range and DSU commands are restricted.
The DSU implements a security filter that monitors the AHB transactions generated by the ARM AHB-AP inside the DAP. If the device is protected, then AHB-AP read/write accesses outside the DSU external address range are discarded, causing an error response that sets the ARM AHB-AP sticky error bits. For more details, refer to the ARM Debug Interface v5 Architecture Specification on www.arm.com.
- Internally from the CPU without any limitation, even when the device is protected
- Externally from a debug adapter with some restrictions when the device is protected
- The first 0x100 bytes form the internal address range
- The next 0x100 bytes form the external address range
When the device is protected, the DAP can only issue MEM-AP accesses in the DSU range 0x0100-0x2000.
The DSU Operating registers are located in the 0x0000-0x00FF area and remapped in 0x0100-0x01FF to differentiate accesses coming from a debugger and the CPU. If the device is protected and an access is issued in the region 0x0100-0x01FF, it is subject to security restrictions. For more information, see Table 1.
When the device is protected, some features that are not activated by APB transactions are unavailable.
| Feature | Code Protected and Unsecured | Code Protected and Secured | Not Code Protected and Unsecured | Not Code Protected and Secured |
|---|---|---|---|---|
| CPU Reset Extension | Yes | Yes | Yes | Yes |
| Clear CPU Reset Extension | No | No | Yes | No |
| Debugger Cold-Plugging | Yes | Yes | Yes | Yes |
| MEM-AP access during Cold-Plugging | No | No | Yes | Yes |
| Debugger Hot-Plugging | No | No | Yes | No |
- Code Protected means FCPN0.CP of the Flash fuse configuration bit is set.
- Secured means SECCFG.DEBUG_LCK bits of the eFuse are non zero values.