36.4.2.6 Stop Condition Timing
A Stop condition occurs when SDA transitions from an Active state to an Idle state while SCL is Idle. Host hardware will issue a Stop condition when it has completed its current transmission and is ready to release control of the bus. A Stop condition is also issued after an error condition occurs, such as a bus time-out, or when a NACK condition is detected on the bus.
After the ACK/NACK sequence of the final byte of the
transmitted/received packet, hardware pulls SCL low for half of an SCL period
(TSCL/2) (see figure below). After the half SCL period, hardware releases
SCL, then samples SCL to ensure it is in an Idle state (SCL =
1
). Host
hardware then waits the duration of the Stop condition setup time (TSU:STO)
and releases SDA, setting the Stop Condition Interrupt Flag (PCIF). If the Stop Condition Interrupt Enable (PCIE) bit is also set, the generic I2CxIF is also set. Important: At least one SCL low
period must appear before a Stop condition is valid. If the SDA line transitions low,
then high again, while SCL is high, the Stop condition is ignored and a Start condition
will be detected by the receiver.
Important:
- At least one SCL low period must appear before a Stop is valid.
- Refer to the “Electrical Specifications” chapter for Stop condition setup and hold times.