Overview
MPLAB ® Code Configurator Melody content for PIC24-dsPIC33 offers device drivers support for Microchip’s PIC24 Microcontrollers (MCUs) and dsPIC33 Digital Signal Controllers (DSCs).
1 Operating Environment
MCC Melody is supported in both MPLAB® X and MPLAB® Xpress
MPLAB® X Operating Environment
- MPLAB® X IDE v5.5.0 or later
- MPLAB® XC16 Compilers v1.70 or later
- MCC Plugin v5.0.0 or later
- MCC Core 5.3.0 or later
MPLAB® Xpress Operating Environments
- MPLAB® Xpress Cloud-based IDE
- Supported Browsers
-
- Google Chrome
- Mozilla Firefox
- Internet Explorer
- Safari
MPLAB® X or MPLAB® Xpress, Supported Operating Systems
- Windows OS
- Linux OS
- MAC OS
2 Documentation Support
- MCC User Guide - Explains the overall MCC usage and has pointers to MCC Melody Content type specific help.
- MCC Content Manager Help - Provided information about MCC Content Manager.
- MCC Melody Technical Reference - Provides detailed technical information about MCC Melody.
- Release notes are available for each component(s) in MCC Content Manager.
- Individual release information is available for each version of the component in the MCC Content Manager in the Version selection dropdown. Example: OPAMP Driver Change Log.
- API Documentation is available for each component through the Resource Management View.

Refer to the individual Component Changelog from Content Manager for the Feature Support, Bug fix information of respective Driver, PLIB Hardware Peripheral, PIC24-dsPIC-Device Releases .

To know how to get the detailed information of individual Component Release version, refer the MCC Content Manager Reference.
3 Installation Requirements
The PIC24/dsPIC33 MCC Melody content such as Drivers, PLIBs, Hardware Peripherals and PIC24/dsPIC device can be installed using the Content Manager.
For more information about the content manager, go to the MCC Content Manager Reference.
4 What's New?
- Drivers
- PLIBs
- Hardware Peripheral Initializer
- PIC24/dsPIC-Devices
Drivers
- Most of the drivers provide portabability to the functionalities of the hardware peripheral.
- Migrate-able across devices and provides usable code and configuration
Multiple Drivers for One Hardware Peripheral
| Driver(s) | Hardware Peripheral Functionality (PLIBs) |
|---|---|
| IC, Edge Output, Pulse Output, PWM | MCCP/SCCP |
| CAN FD and CAN 2.0 | CAN |
| I2C Host, I2C Client | I2C |
| SPI Host, SPI Client | SPI |
Same Driver for Different Hardware Peripherals
The Driver(s) carefully abstracts out the underlying hardware peripheral details, while providing the functionality.
For Ex. Timer Driver can work either with a Timer peripheral or an SCCP peripheral whichever is supported by the device.
Revamped System Module
Getting an appropriate clock source is always a challenging task, however with the new design of System Module, now it all takes a single input from the user of the required clock frequency and MCC helps the user in getting the requested frequency or the closest frequency that's supported while having the corresponding configurations done at the backend.
Generated Firmware
The generated firmware from the Driver(s) supports portability across multiple MCU devices independent of both a peripheral instance, and the MCU device.


Fig 1 : MCC Generated files for Timeout Driver and generated Timer API's
Hardware Peripheral Initializers
The hardware peripheral intializers are generated for bare metal development and provide non-portable direct access to the hardware registers.
The Initialize function has code comments to describe the settings made.

Fig 2: Only 1 function is generated for Hardware Peripheral Initializers
5 Suppported MCU Family Devices
Refer to the below table for the list of device familes supported in both MCC Classic and MCC Melody
| Sl. No. | Device Family | MCC Melody | MCC Classic |
|---|---|---|---|
| 1 | dsPIC33CK512MPT608 |
![]() |
![]() |
| 2 | dsPIC33CK1024MP710 |
![]() |
![]() |
| 3 | dsPIC33CK256MC506 |
![]() |
![]() |
| 4 | dsPIC33CK512MP608 |
![]() |
![]() |
| 5 | dsPIC33CK256MP508 |
![]() |
![]() |
| 6 | dsPIC33CK64MP105 |
![]() |
![]() |
| 7 | dsPIC33CK64MC105 |
![]() |
![]() |
| 8 | dsPIC33CH128MP508 and dsPIC33CH128MP508S1 |
![]() |
![]() |
| 9 | dsPIC33CH512MP508 and dsPIC33CH512MP508S1 |
![]() |
![]() |
| 10 | dsPIC33CH1024MP712 and dsPIC33CH1024MP712S1 |
![]() |
![]() |
| 11 | dsPIC33EP512MU814 |
![]() |
![]() |
| 12 | dsPIC33EP128GS806 |
![]() |
![]() |
| 13 | dsPIC33EP64GS506 |
![]() |
![]() |
| 14 | dsPIC33EP32GS202 |
![]() |
![]() |
| 15 | dsPIC33EP512GM710 |
![]() |
![]() |
| 16 | dsPIC33EP512GP506 |
![]() |
![]() |
| 17 | dsPIC33EV256GM106 |
![]() |
![]() |
| 18 | dsPIC33EV256GM006 |
![]() |
![]() |
| 19 | PIC24F16KM204 |
![]() |
![]() |
| 20 | PIC24FV32KA302 |
![]() |
![]() |
| 21 | PIC24FJ128GA010 |
![]() |
![]() |
| 22 | PIC24FJ64GA004 |
![]() |
![]() |
| 23 | PIC24FJ64GB004 |
![]() |
![]() |
| 24 | PIC24FJ64GA104 |
![]() |
![]() |
| 25 | PIC24FJ256GB110 |
![]() |
![]() |
| 26 | PIC24FJ256GA110 |
![]() |
![]() |
| 27 | PIC24FJ256DA210 |
![]() |
![]() |
| 28 | PIC24FJ256GB210 |
![]() |
![]() |
| 29 | PIC24FJ128GA310 |
![]() |
![]() |
| 30 | PIC24FJ128GB204 |
![]() |
![]() |
| 31 | PIC24FJ128GA204 |
![]() |
![]() |
| 32 | PIC24FJ128GC010 |
![]() |
![]() |
| 33 | PIC24FJ256GB412 |
![]() |
![]() |
| 34 | PIC24FJ256GA412 |
![]() |
![]() |
| 35 | PIC24FJ1024GB610 |
![]() |
![]() |
| 36 | PIC24FJ1024GA610 |
![]() |
![]() |
| 37 | PIC24FJ256GA705 |
![]() |
![]() |
| 38 | PIC24FJ128GL306 |
![]() |
![]() |
| 39 | PIC24FJ512GU410 |
![]() |
![]() |
| 40 | PIC24FJ64GU205 |
![]() |
![]() |
| 41 | PIC24F16KM204 |
![]() |
![]() |
| 42 | PIC24FV32KA302 |
![]() |
![]() |
6 Table: Peripheral Support by MCU Device
The MCC Melody supports the following PIC24/dsPIC33 devices and hardware peripherals:
| Symbol | Note |
|---|---|
![]() |
Peripheral supported |
![]() |
Peripheral presently not supported |
| … | Peripheral does not exist in the device |
| Device | Integrated Analog | Waveform Control | Clocks and Timers | Safety and Monitoring | Wired Communications | System Flexibility | User Interface | Memory | ||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| ADC | CVRef | DAC | CMP | OPA | PGA | CCS | CBG | MCCP | PWM | IC | OC | DSM | TMR | RTCC | QEI | LVD | DMT | WDT | CRC | CAN | I2C | SPI | MSSP | USB | SENT | PMP | UART | CLC | Ext Int | DMA | PTG | LCD | GFX | CTMU | FLASH | |
| dsPIC33CK256MP508 Family | ||||||||||||||||||||||||||||||||||||
| dsPIC33CK128MP202 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK128MP203 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK128MP205 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK128MP206 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK128MP208 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK128MP502 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK128MP503 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK128MP505 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK128MP506 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK128MP508 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK256MP202 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK256MP203 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK256MP205 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK256MP206 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK256MP208 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK256MP502 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK256MP503 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK256MP505 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK256MP506 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK256MP508 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK32MP202 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK32MP203 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK32MP205 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK32MP206 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK32MP502 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK32MP503 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK32MP505 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK32MP506 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK64MP202 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK64MP203 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK64MP205 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK64MP206 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK64MP208 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK64MP502 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK64MP503 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK64MP505 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK64MP506 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK64MP508 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK64MP105 Family | ||||||||||||||||||||||||||||||||||||
| dsPIC33CK32MP102 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK32MP103 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK32MP105 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK64MP102 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK64MP103 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK64MP105 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK64MC105 Family | ||||||||||||||||||||||||||||||||||||
| dsPIC33CK32MC102 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK32MC103 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK32MC105 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK64MC102 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK64MC103 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK64MC105 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CK512MP608 Family | ||||||||||||||||||||||||||||||||||||
| dsPIC33CK256MP305 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK256MP306 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK256MP308 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK512MP305 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK512MP306 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK512MP308 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK256MP605 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK256MP606 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK256MP608 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK512MP605 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK512MP606 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK512MP608 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK256MC506 Family | ||||||||||||||||||||||||||||||||||||
| dsPIC33CK256MC506 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK256MC505 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK256MC503 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK256MC502 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK128MC506 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK128MC505 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK128MC503 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK128MC502 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK256MC106 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK256MC105 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK256MC103 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK256MC102 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK128MC106 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK128MC105 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CK128MC103 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK128MC102 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK1024MP710 Family | ||||||||||||||||||||||||||||||||||||
| dsPIC33CK256MP705 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK256MP706 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK256MP708 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK256MP710 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK512MP705 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK512MP706 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK512MP708 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK512MP710 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK1024MP705 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK1024MP706 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK1024MP708 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK1024MP710 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CK256MP405 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK256MP406 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK256MP408 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK256MP410 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK512MP405 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK512MP406 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK512MP408 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK512MP410 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK1024MP405 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK1024MP406 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK1024MP408 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK1024MP410 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK512MPT608 Family | ||||||||||||||||||||||||||||||||||||
| dsPIC33CK512MPT608-I/PT | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CK256MPT608-I/PT | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH128MP508 Family | ||||||||||||||||||||||||||||||||||||
| dsPIC33CH128MP202 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CH128MP203 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CH128MP205 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CH128MP206 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CH128MP208 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CH128MP502 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CH128MP503 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CH128MP505 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CH128MP506 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CH128MP508 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CH64MP202 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CH64MP203 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CH64MP205 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CH64MP206 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CH64MP208 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CH64MP502 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CH64MP503 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CH64MP505 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CH64MP506 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CH64MP508 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CH128MP508S1 Family | ||||||||||||||||||||||||||||||||||||
| dsPIC33CH128MP202S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH128MP203S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH128MP205S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH128MP206S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH128MP208S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH128MP502S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH128MP503S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH128MP505S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH128MP506S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH128MP508S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH64MP202S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH64MP203S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH64MP205S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH64MP206S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH64MP208S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH64MP502S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH64MP503S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH64MP505S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH64MP506S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH64MP508S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||
| dsPIC33CH512MP508 Family | ||||||||||||||||||||||||||||||||||||
| dsPIC33CH256MP205 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CH256MP206 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CH256MP208 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CH256MP505 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CH256MP506 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CH256MP508 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CH512MP205 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CH512MP206 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CH512MP208 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||
| dsPIC33CH512MP505 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CH512MP506 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CH512MP508 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||
| dsPIC33CH512MP508S1 Family | ||||||||||||||||||||||||||||||||||||
| dsPIC33CH256MP205S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||
| dsPIC33CH256MP206S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||
| dsPIC33CH256MP208S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||
| dsPIC33CH256MP505S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||
| dsPIC33CH256MP506S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||
| dsPIC33CH256MP508S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||
| dsPIC33CH512MP205S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||
| dsPIC33CH512MP206S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||
| dsPIC33CH512MP208S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||
| dsPIC33CH512MP505S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||
| dsPIC33CH512MP506S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||
| dsPIC33CH512MP508S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||
| dsPIC33CH1024MP712 Family | ||||||||||||||||||||||||||||||||||||
| dsPIC33CH512MP705 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CH512MP706 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CH512MP708 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CH512MP710 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CH512MP712 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CH1024MP705 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CH1024MP706 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CH1024MP708 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CH1024MP710 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CH1024MP712 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CH512MP605 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CH512MP606 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CH512MP608 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CH1024MP605 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CH1024MP606 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CH1024MP608 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | |||||||||||||||||||||||
| dsPIC33CH512MP405 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP406 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP808 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP410 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP412 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP405 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP406 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP408 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP410 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP412 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP305 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP306 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP308 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP305 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP306 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP308 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP712S1 Family | ||||||||||||||||||||||||||||||||||||
| dsPIC33CH512MP705S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP706S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP708S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP710S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP712S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP705S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP706S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP708S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP710S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP712S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP605S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP606S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP608S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP605S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP606S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP608S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP405S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP406S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP808S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP410S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP412S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP405S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP406S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP408S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP410S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP412S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP305S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP306S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH512MP308S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP305S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP306S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||
| dsPIC33CH1024MP308S1 | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ... | ||||||||||||||||||||||