9.3 Application Example
After a device Reset, the RCON register can be examined by initialization code to confirm the source of the Reset. In certain applications, this information can be used to take appropriate action to correct the problem that caused the Reset to occur.
All Reset status bits in the RCON register should be cleared after reading them to ensure the RCON value will provide meaningful results after the next device Reset.
Determining the Source of Device Reset illustrates how to determine the source of device Reset using the RCON register.
Determining the Source of Device Reset
int main(void)
{
//... perform application specific startup tasks
// next, check the cause of the Reset
if(RCON & 0x0003)
{
// execute a Power-on Reset handler
// ...
}
else if(RCON & 0x0002)
{
// execute a Brown-out Reset handler
// ...
}
else if(RCON & 0x0080)
{
// execute a Master Clear Reset handler
// ...
}
else if(RCON & 0x0040)
{
// execute a Software Reset handler
// ...
}
else if (RCON & 0x0200)
{
// execute a Configuration Mismatch Reset handler
// ...
}
else if (RCON & 0x0010)
{
// execute Watchdog Time-out Reset handler
// ...
}
// ... perform other application-specific tasks
while(1);
}