14.2 Features

The CAN FD module has the following features:

General

  • Nominal (Arbitration) Bit Rate up to 1 Mbps
  • Data Bit Rate up to 8 Mbps
  • CAN FD Controller Modes:
    • Mixed CAN 2.0B and CAN FD mode
    • CAN 2.0B mode
  • Conforms to ISO 11898-1:2015

Message FIFOs

  • 7 FIFOs Configurable as Transmit or Receive FIFOs
  • One Transmit Queue (TXQ)
  • Transmit Event FIFO (TEF) with a 32-Bit Timestamp

Message Transmission

  • Message Transmission Prioritization:
    • Based on priority bit field and/or
    • A message with the lowest ID is transmitted first using the TXQ
  • Programmable Automatic Retransmission Attempts: Unlimited, Three Attempts or Disabled

Message Reception

  • 16 Flexible Filter and Mask Objects
  • Each Object can be Configured to Filter either:
    • The standard ID and first 18 data bits or
    • The extended ID
  • 32-Bit Timestamp
  • The CAN FD Bit Stream Processor (BSP) implements the Medium Access Control (MAC) of the CAN FD protocol described in ISO 11898-1:2015. It serializes and deserializes the bit stream, encodes and decodes CAN FD frames, manages medium access, Acknowledges frames, and detects and signals errors.
  • The TX handler prioritizes the messages that are requested for transmission by the 
transmit FIFOs. It uses the RAM interface to fetch the transmit data from RAM and provides them to the BSP for transmission.
  • The BSP provides received messages to the RX handler. The RX handler uses an 
acceptance filter to filter the messages that shall be stored in the receive FIFOs. It uses the RAM interface to store received data into RAM.
  • Each FIFO can be configured either as a transmit or receive FIFO. The FIFO control keeps track of the FIFO head and tail and calculates the user address. In a TX FIFO, the user address points to the address in RAM where the data for the next transmit message are stored. In an RX FIFO, the user address points to the address in RAM where the data of the next receive message will be read. The user notifies the FIFO that a message is written to or read from RAM by incrementing the head/tail of the FIFO.
  • The TXQ is a special transmit FIFO that transmits the messages based on the ID of the messages stored in the queue.
  • The TEF stores the message IDs of the transmitted messages.
  • A free-running Time Base Counter (TBC) is used to time-stamp received messages. Messages in the TEF can also be time-stamped.
  • The CAN FD controller module generates interrupts when new messages are received or when messages are transmitted successfully.

Figure 14-2 shows the system block diagram.

Figure 14-2. System Block Diagram