5.7 Resolved Issues
(Ask a Question)The following table lists the customer-reported defects and enhancement requests resolved in Libero SoC v2023.2 that have case numbers. Resolution of previously reported “Known Issues and Limitations” are also noted in this table.
| Case Number | Summary | Resolution |
|---|---|---|
| 01305388 | MPF050T/TS/TL/TLS, MPFS025T/TS/TL/TLS: High-speed I/O clock connectivity update. | See section MPF050T/TS/TL/TLS, MPFS025T/TS/TL/TLS: High-Speed I/O Clock Connectivity Update. |
493642-2616127596, 00935635, 01275935 | PolarFire MPF200T FCVG484: I/O Bank 4 and 5 VDDI DRC. | See section PolarFire MPF200T FCVG484: I/O Banks 4 and 5 VDDI DRC, Design Invalidation. |
| 01241342 | USB library access on Linux prevents the support of multiple eFP6 programmers with Libero/FlashPro Express and SmartDebug. | Added support for multiple eFP6 programmers on the Linux operating system. |
| 01023769 | Reported issue for generic package instantiation. | Resolved the issue for generic package instantiation. |
| 01255870 | Prior to Libero SoC v2023.2, designs targeting PolarFire MPF050T/TS/TL/TLS FPGAs and MPFS025T/TS/TL/TLS SoC could have placed High-Speed I/O Bank Clock (HS_IO_CLK) instances at locations that are not routable. |
See section MPF050T/TS/TL/TLS, MPFS025T/TS/TL/TLS: High-Speed I/O Clock Connectivity Update. |
| 01134983 | Programmable I/O delay update on ports using combined I/O registers. | See section Programmable I/O Delay Update on Ports Using Combined I/O Registers. |
| 01150189 | PF_CCC: PLL solver accuracy. | See section PF_CCC: Improved PLL Solver Accuracy. |
| 01204463 | PF_IOD_OCTAL_DDR: Non-blocking assignments encountered in combinational block. | PF_IOD_OCTAL_DDR core has been updated to address a limiting issue, with no functional change. |
| 00896987 | PF_IOD: OCTAL_PHY differential DQS. | See section PF_IOD: OCTAL_PHY Update. |
| 01254298 |
PF_SOC: MSS: Need to add an ADD/CMD offset in the MSS configurator for DDR3/LPDDR3 and DDR4/LPDDR4. | Added an ADD/CMD offset in the PolarFire SoC MSS configurator for DDR3/LPDDR3 and DDR4/LPDDR4. |
| 493642-2843645269 | SerDes REFCLK pin configuration details. | See section Generate FPGA Array Data - Init Config Report: Add SERDES REFCLK I/O Settings. |
01083419, 1094794 | CoreFIR_PF core generation for the MPFS250T_ES device with a silver license. | CoreFIR_PF core generates properly for the MPFS250T_ES device with a silver license. |
| 01269754 | RTG4_SRAM_AHBL_AXI: Logic issue when two transactions occur consecutively, such that you read from a different slave using AHB, and subsequently attempt to write using this slave. | Resolved logic issue. |
| 01265049 | Support for ISSI IS25LP512M SPI-Flash device with FlashPro 6. | Support has been added for an ISSI IS25LP512M SPI-Flash device with FlashPro 6. |
| 01302899 | Encryption public keys and script availability. | See section Encryption Public Keys and Script. |
| 01227224 | Default TCK frequency for FlashPro 6 during Scan Chain. | Changed the default TCK frequency from 4MHz to 1MHz with FlashPro 6 during Scan Chain. |
| 01278337 | IBIS Term models supported for differential I/Os. | IBIS Term models supported for differential I/Os. |
| 01284803 | RTG4FCCCECALIB DEADLOCK: 50MHz RC Osc Output stuck when ARSTN exposed and GLx set to LOW until PLL locks. | See section RTG4 CCC Improvements. |
| 01257768 | Support for Macronix MX25L25645GSPI-Flash device with FlashPro 6. | Support has been added for a Macronix MX25L25645GSPI-Flash device with FlashPro 6. |
| 01152975 | The jitter report
place_and_route_jitter_report.txt is being
generated with Multipass Place and Route operations. | This issue has been resolved. |
| 01236884 | Ability to disable timing of GB cell. | Added support for wildcard in set_disable_timing. |
| 01108897 | PolarFire PCIe FTS, L0s acceptable latency, PL_TXSWING values are not reflecting in the design initialization report. | In the GUI, the fast training sequence (FTS) and TXSWING options are set to default values and cannot be changed by users. |
| 01236650 | Power estimation for the E51 Monitoring core was missing from the Power Estimator spreadsheet. | This issue has been resolved. |
| 01211657 | Simulation issue with the PF_IOD_GENERIC_TX IP core's TX clock signal. | Fixed a TX clock simulation issue by assigning OE_DATA properly. |
| 01285956 | RTG4 IBIS sub models are not exported in the exported IBIS file. | RTG4 IBIS submodels for DDRIO conditions have been updated. |
| 493642-2663302704 | SmartDebug could not debug design when a non-Microchip device is connected in chain with Microchip device. | SmartDebug can be used to debug design when a non-Microchip device is connected in chain with Microchip device. |
The following table lists the customer-reported defects and enhancement requests resolved in Libero SoC v2023.2 that do not have case numbers. Resolution of previously reported “Known Issues and Limitations” are also noted in this table.
| Summary | Resolution |
|---|---|
| Users cannot export a component description Tcl script for SmartDesign Testbench. | Added support for SmartDesign Testbench to export a component description Tcl script. |
| SmartDesign loses loopback connectivity of the instance when updating the instance port list. | This issue has been resolved: Instance loopback connections are now preserved when an instance port list changes. |
| Bus slices are lost when a new slice is created that overlaps existing ones. | This issue has been resolved: Bus slices are now preserved when creating a new slice with an overlapping range. |
| Jitter reports should state that values are peak-to-peak. | Added a statement in the report header that values are peak-to-peak. |
| PolarFire IBIS Transceiver Reference clock models are not supported. | PolarFire IBIS Transceiver Reference clock models are now supported. |
| The tool crashes when checking constraints when a master clock is invalid. | Added a check to prevent such crashes. |
| Creating or opening a FlashPro Express project should not require hardware to be connected. | This issue has been resolved: A FlashPro Express job project can now be created or opened without requiring a connected programmer. |
| Clarify voptargs required for QuestaSim Pro ME simulation. | Added a QuestaSim Pro ME note in the Libero SoC Simulation Library Setup Instructions about design optimization during simulation. To access this document, go to Pre-Compiled Simulation Libraries, and then click the link for the Libero SoC Design Suite Simulation Library Setup Instructions document. |
|
When min-delay slack is from worst corner, the tap delay inserted on max-delay timing is determined by the min-delay slack. | Best practices recommend that you avoid max-delay timing violation when performing min-delay repair. |