3.7 Resolved Issues
(Ask a Question)The following table lists the customer-reported defects and enhancement requests resolved in Libero SoC v2024.2 that have case numbers. Resolution of previously reported “Known Issues and Limitations” are also noted in this table.
| Case Number | Summary | Resolution |
|---|---|---|
|
493642-570495340, 493642-796226573, 493642-757930812, 01010822, 01248841, 01408429 | set_max_delay and set_min_delay needed added support for static timing analysis of the data path delay without clock path delay. | See section Ignore Clock Latency Constraint on CDC Data Paths. |
| 01476217 | Libero SoC v2024.1 had an issue with IBIS model generation related to the /r character in the IBIS file on Windows operating systems. | This issue has been resolved. |
| 01453580 | Zeroization results could not be read after a ZEROIZE_LIKE_NEW action was completed. | The DEVICE_INFO action has been updated to display the zeroization result/status when the device is in zeroized state. |
| 01453358 | Place and Route fails on designs with heavily congested carry chain clusters. | Place and Route flow has been updated to handle long carry chain clusters for heavily congested designs. |
| 01453038 | The Global Net report failed to list all the non-SET mitigated nets for RTG4 designs. | Each potential input of clock conditioning circuitry is now iterated to find all driving inputs. |
| 01453014 | A warning message appeared for RTG4 SET and non-SET mitigated paths. | The clock conditioning circuitry configuration determines warning conditions. |
| 01452899 | Libero crashed during Design Handoff for debugging for very large designs on Windows operating systems. | SmartDebug data can now be exported for very large designs without causing Libero to crash. |
| 01452099 | Vref pin information did not appear in the Pin Report file. | The Pin Report file now contains Vref pin information. |
| 01443887 | Installer was lacking RHEL 8.x support. | Support for RHEL 8.x has been added to the installer by modifying the supported OS script in the installer. |
| 01439341 | An internal error in m_generic.exe occurred for PolarFire devices, but not for IGLOO2. | This issue has been resolved. |
| 01436755 | Initialize Power Estimator window settings were not getting saved in Microchip Power Estimator. | Initialize Power Estimator now retains the saved settings. |
|
01436743, 01472420 | M2S025T-FCSG158I could not be selected in the SmartFusion2 Power Estimator. | Support has been added for this die-package combination. |
| 01435608 | A persistence issue occurred with the System Builder FDDR when used with DDR3 in 8-bit bus mode. | This issue has been resolved. |
| 01430986 | An issue prevented the synthesis tool from evaluating expressions for designs with enum datatype declarations. | This issue has been resolved. Synthesis now passes satisfactorily for designs with enum datatype declarations. |
| 01429854 | The Tcl commands set_as_target and unset_as_target were not working. | The filetype enum is now set according to the value provided by users in the command. |
| 01428220 | The RECALCULATE ALL button in SmartTime was not active. | This button has been removed. |
| 01423067 | Diff I/O in a bank with Low and Mid values always had a Mid value assigned. | If a combination of Low and Mid input common mode ranges (VCM_RANGE) is used for true differential inputs within the same GPIO bank, the input pairs that also enable the internal 100Ω On-Die Termination (ODT) resistor have a resistor accuracy tolerance percentage that follows the maximum percentage tolerance of the two ranges, per the device datasheet. Mixing VCM_RANGE settings in the same GPIO bank is currently allowed only during post-layout I/O editing. |
| 01422069 | Improved SSN Analyzer DRC violation messages. | The DRC violation message in the Summary tab and the warning message in the Noise Report tab have been updated. |
| 01420458 | For SmartFusion2 and IGLOO2, the VERIFY_DIGEST action did not print the freshly calculated digests. | The VERIFY_DIGEST action has been updated to print freshly calculated digests for Fabric/eNVM when these components are present in the bitstream. |
| 01418457 | An issue occurred with the high-speed serial interface “signal integrity options” configurator. |
The following INFO bubble has been added to have the configurator behavior inform users when they change the TX amp ratio to values other than 1200mV.
|
| 01415931 | A crash could occur when the timing engine analyzed paths without clocks. | This issue has been resolved. |
| 01413236 | LVDS33 IOSTD setting support in Libero was missing for the XCVR REF_CLK. | Libero now supports LVDS33 IOSTD XCVR reference clock pins across PolarFire, PolarFire SoC, and RT PolarFire FPGA devices. |
| 01410800 | A crash resulted from a multi-driver scenario from an intermediate netlist in the Automatic compile point flow. | This issue has been resolved and synthesis now passes satisfactorily. |
| 01409449 | The External Setup value did not consider clock jitter during Maximum Delay Analysis. | The correct jitter value is now added to external delay check calculations. |
| 01402440 | The IBIS model generated by the Libero SoC tool did not contain ODT information for the XCVR_REF_CLK. | xcvr_refclk IBIS models are now exported with default I/O settings. |
|
01389577, 01385119 | When using Mi-V RV32 core, Verilog parameters were observed in the custom HDL+ configurator after modifying the core. | This issue has been resolved. Custom HDL+ core configurators now appear only in the Verilog parameters related to the current core. |
| 01388294 | The reworked clock conditioning circuitry model could not identify that a source pin is a dedicated input pin when using get_ports and get_pins. | Jitter numbers for clock conditioning circuitry constraints now match if either get_ports or get_pins is used. |
| 01373404 | LVPECLE33 was the default IOSTD for bi- and tri-I/Os when users selected LVVCMOS33 as a default I/O technology. | See section Project Setting Default I/O Technology LVCMOS 3.3V. |
| 01371227 | The I/O Constraint Editor Package view crashed when placing a group of signals from Main Object Browser into the view. | This issue has been resolved and the crash no longer occurs. |
| 01369314 | Depending on the user design, I/O glitches could be observed when exiting programming mode. Typically, this occurred at the end of program or verify operation. | The programming algorithms of SmartFusion2, IGLOO2, RTG4, PolarFire, and PolarFire SoC devices have been updated to avoid a potential I/O glitch when exiting programming mode. |
| 01367141 | The MATH block model passed invalid multicycle constraints to timing analysis. | Libero constraint checker has been updated to issue an error message if it encounters any invalid multicycle path constraints. |
| 01363398 | The PF_DDR3 and PF_DDR4 “CK/CA additive offset” value is not passed to the internal RTL logic. | See section “CK/CA additive offset” Parameter in the Training IP of DDR Controllers. |
| 01360180 | Clock-to-clock uncertainty values were not considered during a Min-Delay repair. | This issue has been resolved to address design hold violations. |
| 01358909 | The Power Estimator tool for PolarFire SoC devices did not include MSS I/Os. | MSS I/Os are now supported under the MSS&MDDR tab of the MPE. |
| 01353583 | The reworked model for the RTG4 family did not report the correct path and jitter-estimation values. | In cascaded PLL scenarios, jitter values are now reported without errors. |
| 01327940 | SmartDebug experienced crashes during project creation if the DDC file exceeded 1.5 GB in size. | Crashes are no longer experienced and DDC file sizes up to 2.8GB are supported. |
| 01282955 | SmartDebug users could not control the Security Keys (UPK1 and DPK) in the DDC file. | Users can now control the exporting of Security Keys (UPK1 and DPK) resulting from DDC for the SmartFusion2, IGLOO2, PolarFire FPGA, RT PolarFire, and PolarFire SoC family. |
| 01145463 | A SpaceFibre IP simulation failure could occur with PolarFire when using VCS simulator. | The PF_XCVR simulation model and library have been updated to align TX_DATA properly when LANEx_TX_WCLK is connected to a clock source other than LANE0_TX_CLK_G. |
|
01137352, 01134979, 01319721 | The check for the Place and Route state reverted during the 0th iteration. | The multi-pass layout tool now bypasses Place and Route when it is in the NOT_RUN state and runs the Verify Timing. |
| 01061565 | The reworked clock conditioning circuitry model or jitter estimation addresses the warnings seen with clock conditioning circuitry clocks. | No warnings are shown in Libero.log. |
The following table lists the customer-reported defects and enhancement requests resolved in Libero SoC v2024.2 that do not have case numbers. Resolution of previously reported “Known Issues and Limitations” are also noted in this table.
| Summary | Resolution |
|---|---|
| IGLOO2 IBIS Export for custom temperature range. | Custom temperature ranges are supported in IBIS Export. |
| Streamline IGLOO2 Tamper Macro Zeroization options by removing the Recoverable option. | See section SmartFusion2 and IGLOO2. |
|
Issues were observed with the Python script that injected ECC errors in simulation for RTG4 devices. | Resolved issues with the Python script to inject ECC errors in simulation for RTG4 devices. This includes small RAM depth, multiple RAM instances, and instance name inconsistencies. |