10.5 New Silicon Features and Enhancements
(Ask a Question)10.5.1 PolarFire, RT PolarFire, and PolarFire SoC
(Ask a Question)10.5.1.1 Design Initialization Data and Memory Report
(Ask a Question)Libero SoC v2021.3 consolidates all configuration information into the Design Initialization and Memory report. Tie-off information about important input pins for unused blocks also has been added to this report.
For more information, see AC478: PolarFire FPGAs for Safety-Critical Applications.
10.5.1.2 External Timing Closure of IOD Interfaces
(Ask a Question)The Repair minimum delay violations option of Place & Route in Libero SoC v2021.3 has been enhanced for external timing closure of IOD interfaces. If an initial maximum delay analysis detects any external setup violation, the programmable I/O delays are adjusted by the subsequent passes of minimum delay repair.
10.5.1.3 XCVR ERM Enhancements to Improve Transceiver Robustness
(Ask a Question)The PF_XCVR_ERM core in Libero SoC v2021.3 improves the robustness
of the Enhanced Receiver Management solution where, in rare cases, the link would drop and
then restart.
10.5.1.4 PF_TAMPER SECURITY_LOCKDOWN
(Ask a Question)The PF_TAMPER core version in Libero SoC v2021.3 renames the port
LOCKDOWN to SECURITY_LOCKDOWN. When upgrading
designs containing a PF_TAMPER component from a prior release,
reconnect the net to the new port.
10.5.1.5 PolarFire XCVR-Sourced Fabric Clocks and Jitter Compensation
(Ask a Question)The PolarFire XCVR can source three different clocks into the fabric:
TX_CLKRX_CLKREFCLK(FAB_REF_CLK)
These clocks contain high-frequency jitter that is not automatically considered by Libero in the timing report and SmartTime. It is recommended that users add clock-uncertainty constraints to these clocks in their design. The following table shows recommended values for clock uncertainty per clock, resource, and speed-grade.
| Clock Type | STD | -1 |
|---|---|---|
FAB_REF_CLK on Global | 275 ps | 200 ps |
FAB_REF_CLK on Regional | N/A | N/A |
TX_CLK_G on Global | 300 ps | 225 ps |
TX_CLK_R on Regional | 225 ps | 150 ps |
RX_CLK_G on Global | 325 ps | 250 ps |
RX_CLK_R on Regional | 250 ps | 175 ps |
set_clock_uncertainty -setup 0.150 [ get_pins { PF_XCVR_ERM_LANE2/I_XCVR/LANE0/TX_CLK_R } ]
set_clock_uncertainty -setup 0.175 [ get_pins { PF_XCVR_ERM_LANE2/I_XCVR/LANE0/RX_CLK_R } ]
The following example shows a clock-uncertainty constraint with STD speed grade.
# TX_CLK and RX_CLK on Globals
set_clock_uncertainty -setup 0.300 [ get_pins { PF_XCVR_ERM_LANE2/I_XCVR/LANE0/TX_CLK_G } ]
set_clock_uncertainty -setup 0.325 [ get_pins { PF_XCVR_ERM_LANE2/I_XCVR/LANE0/RX_CLK_G } ]
# FAB_REF_CLK on Global
set_clock_uncertainty -setup 0.275 [get_clocks PF_DDR4_C0_0/CCC_0/pll_inst_0/OUT1]The automatic management of these constraints will be added in a future release of Libero SoC.
10.5.2 PolarFire SoC
(Ask a Question)10.5.2.1 Device Check when Importing an MSS Component (CXZ) into Libero SoC
(Ask a Question)Libero SoC v2021.3 checks against the current project device settings when importing an MSS component (CXZ).
For more information, see the Libero SoC Design Flow User Guide .
10.5.2.2 Export BSDL File
(Ask a Question)Exporting BSDL files is now supported for PolarFire SoC devices in Libero SoC v2021.3.
For more information, see the Libero SoC Design Flow User Guide .
10.5.2.3 Configure I/O States During JTAG Programming Tool Support
(Ask a Question)Libero SoC v2021.3 adds support for the Configure I/O States During JTAG Programming tool for PolarFire SoC devices.
For more information, see the Libero SoC Design Flow User Guide .
10.5.2.4 Invoke MSS Configurator from Libero SoC as Read-Only
(Ask a Question)In a PolarFire SoC project opened in Libero SoC v2021.3, you can now invoke the MSS configurator by double clicking on the MSS component under the Design Hierarchy pane to view the settings of the MSS in read-only mode. To change any setting, you must run the standalone MSS configurator outside of Libero.
For more information, see the Libero SoC Design Flow User Guide .
10.5.2.5 MSS Simulation Model Enhancements
(Ask a Question)Libero SoC v2021.3 enhances the MSS simulation model to add support for the following features:
- DMA-type transfers between MSS and fabric
- Fabric initiator accessing L2-LIM of MSS
For more information, see the Revision History topic in the PolarFire SoC FPGA MSS Simulation User Guide.
10.5.2.6 eNVM System Service
(Ask a Question)The PF_SYSTEM_SERVICES core in Libero SoC v2021.3 adds a service to
read eNVM parameters from PolarFire SoC devices.
For more information, see the Revision History topic in the PolarFire® System Services SgCore User Guide.
10.5.3 RTG4
(Ask a Question)10.5.3.1 SmartDebug FPGA Hardware Breakpoint Area Reduction
(Ask a Question)For RTG4 designs, Libero SoC v2021.3 reduces the area of the logic inserted for FPGA Hardware Breakpoint.