3.3.3.2 If You Have Windows 7, 8, 10 or 11, Use Administrator Mode
To run the MPLAB Device Driver Switcher, you must be in Administrator mode. To run the Switcher utility as administrator, right click on the executable and select Run as Administrator.
The executable is located at:
C:\Program
Files\Microchip\MPLABX\vx.xx\Switcher\64Bit\MPDDSwitch.exe
It is recommended that you use the Switcher GUI utility first to switch the drivers. If this is problematic, you may switch the drivers using command-line applications.
To run the command-line application – mchpdds64.exe –
as administrator, first open the command prompt as administrator: , right click and select Run as Administrator. This
will open up the Administrator: Command Prompt. After this, the instructions provided in
the ReadMe64.txt file may be followed to complete the driver
switching.