53.4 External Analog Reference Connections

The following schematic checklist is only necessary if the application is using one or more of the external analog references. If the internal references are used instead, the following circuits are not necessary.

Figure 53-3. External Analog Reference Schematic With Two References
Figure 53-4. External Analog Reference Schematic With One Reference
Table 53-2. External Analog Reference Connections
Signal NameRecommended Pin ConnectionDescription
VREFA

2.0V to VDDANA - 0.6V for ADC

1.0V to VDDANA - 0.6V for DAC

Decoupling/filtering capacitors: 100nF(1)(2) and 4.7µF(1)

External reference from VREFA pin on the analog port.
VREFB

1.0V to 5.5V for SDADC

Decoupling/filtering capacitors: 100nF(1)(2) and 4.7µF(1)

External reference from VREFB pin on the analog port.
GNDGround
Note:
  1. These values are given as a typical example.
  2. Decoupling capacitor should be placed close to the device for each supply pin pair in the signal group.