5.1 Identifying Product ID and Revision
The revision and product identifier of Xplained Pro boards can be found in two ways; through Atmel Studio or by looking at the sticker on the bottom side of the PCB.
By connecting an Xplained Pro board to a computer with Atmel Studio running, an information window will pop up. The first six digits of the serial number, which is listed under kit details, contain the product identifier and revision. Information about connected Xplained Pro extension boards will also appear in the Atmel Kits window.
The same information can be found on the sticker on the bottom side of the PCB. Most kits will print the identifier and revision in plain text as A09-nnnn\rr where nnnn is the identifier and rr is the revision. Boards with limited space have a sticker with only a QR-code which contains a serial number string.
|
The serial number string has the following format: "nnnnrrssssssssss" n = product identifier r = revision s = serial number |
The kit identifier for SMARTCARD Xplained Pro is 2593.