8.2 Interface to the Model
- Initialize the model in
main.c.
/* Initialize MPLABML Knowledge Pack */ kb_model_init(); - Call the sml recognition function as long as
there are samples (rdcnt) in the
queue.
... while (rdcnt--) { int ret = sml_recognition_run((sample_data_t *) ptr++, NUM_AXES); ... - In app_config.h, ensure the macro
DATA_STREAMER_FORMAT is set to
APP.
// Data streaming formatting selection #ifndef DATA_STREAMER_FORMAT #define DATA_STREAMER_FORMAT DATA_STREAMER_FORMAT_APP #endif - Build and flash to the device.
Note: To see the demo in action, after these steps, follow the Use
Data Visualizer streamer to see the classification.