The figures below illustrate various escape pattern designs.
Figure 4-2. SAMA7G54 Top Layer Example -
SignalFigure 4-3. SAMA7G54 Layer 2 Example -
GroundFigure 4-4. SAMA7G54 Layer 3 Example -
SignalFigure 4-5. SAMA7G54 Layer 4 Example -
PowerFigure 4-6. SAMA7G54 Layer 5 Example -
SignalFigure 4-7. SAMA7G54 Layer 6 Example -
SignalFigure 4-8. SAMA7G54 Layer 7 Example -
GroundFigure 4-9. SAMA7G54 Bottom Layer Example -
Signal
The decoupling capacitors should be placed on the bottom,
as close as possible to the vias connecting the power pins of the MPU. An example of
such placement can be seen in the following figure.
Figure 4-10. SAMA7G54 Decoupling Capacitors
Placement Example
DS00005871D
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.