5.4 How to Use the Hardware Tool Emergency Boot Firmware Recovery Utility
- If the debugger has no LED lit.
- If the procedure described in the previous section was not successful.
YOU MUST HAVE MPLAB X IDE v6.25 OR GREATER TO USE THE EMERGENCY RECOVERY UTILITY FOR MPLAB PICkit Basic.
Carefully follow the instructions found in MPLAB X IDE under the main menu options .
The figure below shows where the emergency recovery button is located on the MPLAB PICkit Basic In-Circuit Debugger. You can use a paperclip or small screwdriver (shown) to press the button.
If the procedure was successful, the recovery wizard displays a success screen. The MPLAB PICkit Basic will now be operational and able to communicate with the MPLAB X IDE.
If the procedure failed, try it again. If it fails a second time, contact Microchip Support at support.microchip.com.