6.1 How Does it Work?
What's in the silicon that allows it to communicate with the MPLAB PICkit Basic In-Circuit Debugger?
Modules in the silicon allow different types of communication interfaces. The MPLAB PICkit Basic In-Circuit Debugger can communicate with a device via the ICSP™ interface or other interfaces using an adapter board(s). If the communication module allows access to the device build-in debug circuitry, the debugger can access this to perform debug functions.
How is the throughput of the processor affected by having to run a debug executive?
For PIC® MCU devices, a debug executive is programmed into program or dedicated memory during a debug session. The debug executive doesn't run when Run Without Debugging is selected, so there is no throughput reduction when running your code; that is, the debugger doesn’t ‘steal’ any cycles from the target device.
Does the MPLAB PICkit Basic In-Circuit Debugger have complex breakpoints like other in-circuit emulators/debuggers?
No. But you can break based on a value in a data memory location or program address.
Does the MPLAB PICkit Basic In-Circuit Debugger have complex breakpoints?
Yes. You can break based on a value in a data memory location. You can also do sequenced breakpoints, where several events have to occur before it breaks. However, you can only do two sequences. You can also do the AND condition and do PASS counts.
Is the MPLAB PICkit Basic In-Circuit Debugger optoisolated or electrically isolated?
No. You cannot apply a floating or high voltage (120V) to the current system.
Will the MPLAB PICkit Basic In-Circuit Debugger slow down the running of the program?
No. The device will run at any device speed as specified in the data sheet.
Is it possible to debug a dsPIC DSC device running at any speed?
The MPLAB PICkit Basic In-Circuit Debugger is capable of debugging at any device speed as specified in the device’s data sheet.