5.1.8.2 SHA - HMAC Digest

The SHA command may be used to calculate an HMAC Digest instead of an SHA256 Digest. The procedure is essentially the same but requires the use of an internal key and the use of HMAC_START instead of START.

The following procedure is used when no context switching is required:
  1. Issue the SHA command in HMAC_Start mode with key location indicated. No message is included.
  2. Issue the SHA command in Update mode with 1 to 64 bytes of the message.
  3. Repeat step 2 until the total number of bytes of the message has been submitted.
  4. Issue the SHA command in End mode to complete the HMAC Digest calculation.
Table 5-33. Input Parameters SHA HMAC Mode

Opcode
(1 Byte)

Mode
(1 Byte)

Param2
(2 Bytes)

Data
(Varies by Mode)

Description
0x470x040x00 0[slot]0 bytesHMAC Start mode and include a key from a data slot
0x040xFF FF0 bytesHMAC Start mode and include a key from TempKey
0x010x00 [ByteCount]1 to 64 bytesUpdate mode
0x020x00 [ByteCount]0 to 64 bytes

Finalize mode:  Digest placed in Output Buffer and TempKey

0x420x00 [ByteCount]Finalize mode: Digest placed in Output Buffer and Message Digest Buffer
0xC20x00 [ByteCount]Finalize mode: Digest placed in Output Buffer only
Table 5-34. Output Response SHA256 Standard
NameModeSizeDescription
Response0x04, 0x011 byte0x00 if successful, otherwise an error code is received
0x02, 0x42, 0xC2

1 byte
32 bytes

If Error Code
HMAC Digest upon success