3.3.6 Programming Commands

To display information about the programming commands available in the MDB, type help programming. The following table provides additional information for these commands.

Important: The set command, including the tool property options, must be executed before the Hwtool command is issued, otherwise the changes to the tool properties will be ignored.
Table 3-10. Programming Commands
CommandDescription
DumpWrites the device memory to a hex file.

Command format:

Dump [-m] filename

The m is an optional argument that specifies which memories to write to the hex file. It can be any combination of the following:

  • p - Program Memory (Flash)
  • e - EE Data
  • c - Configuration Bits
  • u - User ID memory
  • b - Boot Memory
  • f - Flash Data

The filename is the full path and name to the hex file.

ExecuteExecute the specified function from the loaded script.

Command format:

Execute fuctionname

LoadScriptLoad the target script.

Command format:

LoadScript scriptname

ProgramPrograms device memory with the image specified by the file. If you program with a HEX file and want to do debug run as in IDE, you will need to add -debug option.
Note: If the path or filename has spaces in it, you must use the quotation marks. If there are no spaces in the path of filename, the quotation marks are not needed, as shown below.

Command format:

Program executableImageFile [-debug]

UploadUploads the executable image to MDB memory.

The source of the instructions to be loaded is the contents of the memory of an attached PIC® device through the programmer or debugger.

Command format:

Upload