1.2 Warnings

  • This Midspan should only be connected to an IP device with which it was bought. Using PD-9501GC with other IP devices can cause damage to IP device.
  • Follow basic electricity safety measures whenever connecting PD-9501GC to its power source.
  • A voltage mismatch can cause equipment damage and may pose a fire hazard. If voltage indicated on the label is different from the power outlet voltage, do not connect PD-9501GC to this power outlet.
Warning: Do not use a cross-over cable between the PD-9501GC output port and the load device.