1.23 USART Driver Asynchronous - USART Echo
This example echoes the received characters over the console using the USART driver in asynchronous mode.
Description
This example uses the USART driver in asynchronous mode in Bare-Metal and RTOS environment to communicate over the console. It receives and echo’s back the characters entered by the user.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/driver/usart/async/usart_echo/firmware.
To build the application, refer to the following table and open the project using its IDE.
Project Name | Description |
---|---|
sama5d29_curiosity.X | MPLABX project for SAMA5D29 Curiosity Development Board |
sam_a5d27_som1_ek.X | MPLABX project for SAMA5D27-SOM1-EK1 |
Setting Up AT91Bootstrap loader
To load the application binary onto the target device, we need to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.
Setting Up the Hardware
The following table shows the target hardware for the application projects.
Project Name | Description |
---|---|
sama5d29_curiosity.X | SAMA5D29 Curiosity Development Board |
sam_a5d27_som1_ek.X | SAMA5D27-SOM1-EK1 |
Setting Up SAMA5D27-SOM1-EK1
- Short jumper JP2 (DEBUG_DIS)
- Connect the Debug USB port on the board to the computer using a micro USB cable
Setting Up SAMA5D29 Curiosity Development Board
- Connect a FTDI cable from UART Debug (J28) port to computer.
- Connect the USB_A port on board to the computer using a USB-C type cable.
Running the Application
- Build the application using its IDE
- Open the Terminal application (Ex.:Tera term) on the computer.
- Connect to the EDBG/Jlink Virtual COM port and configure the serial settings as
follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
- Type a character and observe the output on the console as shown below:
- LED toggles each time the character is echoed
Board | LED Name |
---|---|
SAMA5D27-SOM1-EK1 | D5 (Green) |
SAMA5D29 Curiosity Development Board | RGB_LED (Green) |