1.1.22 PIC32CX-BZ3 and WBZ35x Curiosity Board: Building and Running the I2C Bootloader Applications
Building the Application
Path of the application within the repository is apps/i2c_bootloader/.
To build the application, refer to the following table and open the project using its IDE.
Bootloader Application
| Project Name | Description |
|---|---|
| bootloader/firmware/wbz351_curiosity.X | MPLAB X Project for PIC32CX-BZ3 and WBZ35x Curiosity Board |
Test Application
| Project Name | Description |
|---|---|
| test_app/firmware/wbz351_curiosity.X | MPLAB X Project for PIC32CX-BZ3 and WBZ35x Curiosity Board |
Setting Up PIC32CX-BZ3 and WBZ35x Curiosity Board
-
SAM E54 Xplained Pro Evaluation Kit is used for Host development kit and PIC32CX-BZ3 and WBZ35x Curiosity Board is used for Target development kit

-
Connect the pin 11 of EXT3 of the Host development kit to the I2C SDA (PA13) line on mikroBUS (J4) of the Target development kit
-
Connect the pin 12 of EXT3 of the Host development kit to the I2C SCL (PA14) line on mikroBUS (J4) of the Target development kit
-
Connect a ground wire between the Host development kit and Target development kit
-
Connect the Debug USB port on the Host development kit to the computer using a micro USB cable
-
Connect the Debug USB port on the Target development kit to the computer using a micro USB cable
Building and Configuring I2C Host Application
Using I2C SDCARD Host Application to Send the Application Binary to Target Development Kit

If the SDCARD Host development kit being used is other than SAM E54 Xplained Pro Evaluation Kit then follow the steps mentioned in Configuring the SDCARD Host Applications.
-
Open the SDCARD host application project host_app_sdcard/firmware/sam_e54_xpro.X in the IDE.
- If a SDCARD host application project of different development kit is used then open that project in the IDE
-
Build and program the SDCARD host application using the IDE on to the I2C Host development kit.
-
Open the test application project test_app/firmware/wbz351_curiosity.X in the IDE.
-
Build the project to generate the binary (Do not program the binary).
-
Copy the application binary into the SD card and insert the SD card in the SD card slot available on the SAM E54 Xplained Pro Evaluation Kit.
-
Open the Terminal application (e.g., Tera Term) on the computer.
-
Configure the serial port settings for Host development kit as follows:
- Baud: 115200
- Data: 8 Bits
- Parity: None
- Stop: 1 Bit
- Flow Control: None
-
Jump to Running the Application.
Running the Application
-
Open the bootloader project bootloader/firmware/wbz351_curiosity.X in the IDE.
-
Build and program the application using the IDE on to the Target development kit.
- RGB_LED_GREEN will be turned-on to indicate that bootloader code is running on the target
- RGB_LED_GREEN will also turn on when the bootloader does not find a valid application; i.e., the first word of the application (stack pointer), contains 0xFFFFFFFF
-
If the test application is being programmed, open the Terminal application (e.g., Tera Term) on the computer and configure the serial port settings for Target development kit as follows:
- Baud: 115200
- Data: 8 Bits
- Parity: None
- Stop: 1 Bit
- Flow Control: None
-
Press the Switch SW0 on the Host development kit to trigger programming of the application binary.
-
Once the programming is complete:
-
LED0 on the Host development kit will be turned on indicating success
-
If SDCARD Host application was used to program the application binary following message will be displayed on the terminal of Host development kit

-
-
If the above step is successful, press the Reset button on Target development kit. The RGB_LED_GREEN should then begin blinking.
-
The Target development kit will be reset. Upon re-start, the bootloader will jump to the user application.
-
If the test application is programmed then RGB_LED_GREEN should start blinking and the user should see below output on the Target development kit console

-
-
Press and hold the Switch SW3 on Target development kit to trigger Bootloader from test application and the user should see below output and then press the Reset button.

-
Press Reset button on the Host development kit to reprogram the application binary.
-
Repeat Steps 4-6 once.
- This step is to verify that bootloader is running after triggering bootloader from test application in Step 6
Additional Steps
Using SDCARD Host Application
-
If multiple Target development kit are to be programmed using the same Host development kit then refer to the Configuring the SDCARD Host Applications
-
Once done, repeat the applicable steps mentioned in Running the Application