2 Touch Configurator Release Notes
Touch Library v3.17.0 Release
NEW FEATURES SUPPORTED
- Added Touch Library support for PIC32CM-GC/SG devices.
- Added Touch Library support for PIC32WM_BZ6 devices.
- Improved Mutual Capacitance pin assignment UI.
- Resolved issue related to the lump feature support in Touch configurator UI.
- Resolved compilation issues in Timer-based driven shield project generation for SAM D10, SAM D11.
Projects created for the PIC32WM_BZ6 device are currently experiencing compilation issues with the existing compiler (v4.45). Please await the next compiler release (v4.60), which will include a resolution for this problem.
DEVELOPMENT TOOLS
- MPLAB® X IDE v6.20 or higher
- MPLAB® XC32 C/C++ Compiler v4.45
- MPLAB® X IDE plug-ins:
- MPLAB® Code Configurator (MCC)
- MCC Plugin v5.5.1
Touch Library v3.16.0 Release
NEW FEATURES SUPPORTED
- Added Touch Library support for PIC32CK SG/GC devices.
- Updated acquisition library files for SAMC2x and PIC32CMJH device families.
- Improved Matrix View for Mutual Capacitance pin assignment.
- Fixed the software low power sensor's node mask re-generation issue.
- Resolved dependency issues in Timer-based driven shield project generation for SAM C2x, SAM L22.
- For Arm® Cortex-M TrustZone® devices, RTC configured by Touch didn't work. Workaround: Call touch_init after RTC_Initialize in the SYS_Initialize function.
- For Arm® Cortex-M TrustZone® devices, few Touch lines are inoperative due to the default configuration bits set during initialization. Workaround: Manually modify the configuration bits.
- For Arm® Cortex-M TrustZone® devices, there is a code compilation error when the boost mode feature is selected. Workaround: Library files have to be manually pasted in the specified path.
- MPLAB® X IDE v6.20
- MPLAB® XC32 C/C++ Compiler v4.40
- MPLAB® X IDE plug-ins:
- MPLAB® Code Configurator (MCC)
- MCC Plugin v5.5.1
- MCC Harmony Core v1.5.2
Touch Library v3.15.0 Release
NEW FEATURES SUPPORTED
- Touch Library support has been added for the PIC32MZ2051W104132.
- Improved the Matrix View for Mutual Capacitance pin assignment.
- Added an option to update all parameters of the same category in the sensor parameters table.
- Improved visibility of the Horizontal Scrollbar.
- Fixed the bugs related to the Driven Shield configuration for the SAMD21.
- Fixed the issue with the selection of a 1T surface without gesture option.
- Fixed the code generation issue with the Boost mode and surface combination.
- Fixed the PIC32MZDA code compilation issue.
- Fixed the PIC32CZCA software low power compilation issue.
- Fixed the Configuration Summary screen for the PIC32CMLE.
- Fixed the issue with surface pin configuration getting swapped on re-opening Touch configurator.
- Timer based driven shield project may not work for SAM C2x, SAM L22.
- Compilation error in SAML11 Boost Mode project.
- MPLAB® X IDE v6.20
- MPLAB® XC32 C/C++ Compiler v4.35
- MPLAB® X IDE plug-ins:
- MPLAB® Code Configurator (MCC)
- MCC Plugin v5.5.0
- MCC Harmony Core v1.5.1
Touch Library v3.14.0 Release
NEW FEATURES SUPPORTED
- MISRA-C 2012 Mandatory and Required rules Compliance achieved for Harmony generated Touch files.
- Touch Configurator is upgraded to the latest framework.
- Touch Tuning (bidirectional) support is extended for Surface and Gesture features from Touch plugin version 2.2.0.
- SAM D51, E5x acquisition libraries are updated to version 1.5 to fix a bug regarding acquisition module getting struck.
- Fixed the bug to configure more than 3 steps in frequency hop UI.
- Fixed the bug related to SAMD20 Driven Shield Plus.
- MPLAB® X IDE v6.10
- MPLAB® XC32 C/C++ Compiler v4.30
- MPLAB® XIDE plug-ins:
- MPLAB® Code Configurator (MCC)
- MCC Plugin v5.3.7
- MCC Harmony Core v1.3.2
- Harmony 3 – Harmony Services – v1.3.1(mandatory)
- MPLAB® Code Configurator (MCC)
Touch Library v3.13.1 Release
BUG FIXES
- Fixed bug related to SERCOM getting disconnected from Touch Library component when MCC is closed.
- Software based low power code compilation error is fixed.
- Sleep code moved to touch_example template.
- Fixed bug related to PTC mask being disabled for PIC32CMJH device.
- Updated SAML1x and PIC32CM LE00/LS00/LS60 device acquisition libraries for bug fix related to overwriting PORT_MUX registers for pins adjacent to touch pins.
- Touch Configurator summary page update for displaying versions of few acquisition libraries.
Touch Library v3.12.1 Release
NEW FEATURES SUPPORTED
Touch Tune tab provides information to user on bidirectional or unidirectional interface.
BUG FIXES
- Fixed bug related to CSD option shown for devices which doesn't have CSD feature.
- Driven shield on SAMD2x wasn't working correctly. This is fixed.
- Bug related to gesture timing periodicity is fixed.
- Scroller configuration related bug is fixed in GUI.
- Unintended braces in touch timer function is removed.
- SAMD2x Low power related issues are fixed.
- For PIC32CM JH and SAMC2x families, event system based low power has issues when it enters low power mode. Workaround - Use software based low power feature.
- For SAML1x and PIC32CM LE00/LS00/LS60 device families, PORT_MUX registers for pins adjacent to touch pins may be overwritten by touch library.
- MPLAB® X IDE v6.05
- MPLAB® XC32 C/C++ Compiler v4.20
- MPLAB® XIDE plug-ins:
- MPLAB® Code Configurator (MCC)
- MCC Plugin v5.2.2
- MCC Core v5.4.14
- MPLAB® Code Configurator (MCC)
- Bug related to enabling Drivenshield is resolved
- MPLAB® X IDE v6.00
- MPLAB® XC32 C/C++ Compiler v4.10
- MPLAB® XIDE plug-ins:
- MPLAB® Code Configurator (MCC)
- MCC Plugin v5.1.9
- MCC Core v5.4.4
- MPLAB® Code Configurator (MCC)
Touch Library v3.12.0 Release
NEW FEATURES SUPPORTED
- PIC32CM JH family device support is done.
- RTC CountSync is disabled by default for all touch projects.
- Goto menu for Touch Configurator is set to proper path.
- Event system based low power has issues when it enters low power mode.
- MPLAB® X IDE v6.00
- MPLAB® XC32 C/C++ Compiler v4.10
- MPLAB® XIDE plug-ins:
- MPLAB® Code Configurator (MCC)
- MCC Plugin v5.1.4
- MCC Core v5.4.3
- MPLAB® Code Configurator (MCC)
Touch Library v3.11.2 Release
BUG FIXES
- Bug related to Touch Configurator not opening in MPLAB® Code Configurator (MCC) is resolved. Prerequisite MCC Plugin v5.1.2 and MCC Harmony Core v1.1.0.
- Touch files not properly added to project for Trustzone applications. This is resolved.
- The protocol version used in TouchTune.c file is updated to match with MPLAB® Touch Plugin v2.0.0.
- Touch tune data with MPLAB® Touch Plugin does not work with Boost mode.
- MPLAB® X IDE v6.00
- MPLAB® XC32 C/C++ Compiler v4.00
- MPLAB® XIDE plug-ins:
- MPLAB® Harmony Configurator (MHC) v3.8.3
- MPLAB® Code Configurator (MCC)
- MCC Plugin v5.1.2
- MCC Harmony Core v1.1.0
Touch Library v3.11.1 Release
BUG FIXES
- Bug related to SAME5x Prescaler is resolved.
- Bug related to Touch timer periodicity is resolved.
- Data Streamer tune data is sent only once after each touch measurement.
- Compilation error on SAMD10 device is resolved.
- Boost mode libraries and API files are NOT added when Boost mode is enabled. This is resolved.
- Touch tune data with MPLAB Touch Plugin does not work with Boost mode.
- MPLAB X IDE v6.00
- MPLAB XC32 C/C++ Compiler v4.00
- MPLAB XIDE plug-ins:
- MPLAB Harmony Configurator (MHC) v3.8.2
Touch Library v3.11.0 Release
NEW FEATURES SUPPORTED
- Two-way debug protocol is supported.
- Now user can select between MPLAB Data Visualizer Touch plugin and old Data Visualizer in the Parameters->Tune tab of Touch Configurator.
- Refer to Introduction to Touch Plugin for more details on MPLAB Data Visualizer Touch Plugin.
- Bug related to mutual cap surface sensor node generation is fixed
- Error related to surface two-way debug files are fixed
- Label related issue in Mutual cap table view pin selection is fixed
- MPLAB X IDE v5.50
- MPLAB XC32 C/C++ Compiler v2.41
- MPLAB XIDE plug-ins:
- MPLAB Harmony Configurator (MHC) v3.8.2
- csp v3.10.0
- mhc v3.8.2
- Touch Configurator does not work properly when configuring Slider/Wheel using MCC Harmony Library. Workaround is to use Harmony Configurator.
Touch Library v3.10.1 Release
BUG FIXES
- Low-power related bug fixes for SAMD1x and software low-power
- Touch Library's capability name is reverted back to "TouchData"
- Bug fix related to resistor value not populated on node parameter for Mutual cap sensor
- MPLAB X IDE v5.50
- MPLAB XC32 C/C++ Compiler v3.01
- MPLAB X IDE plug-ins:
- MPLAB Harmony Configurator (MHC) v3.8.0
Touch Library v3.10.0 Release
NEW FEATURES SUPPORTED
- Driven shield support extended for - SAM D1x, SAM D20
- Acquisition engine and library are separate in MHC project graph
- PIC32MZDA device support
- SAMHA1 ondemand Osc8m ondemand not set
- ATSAMD10D14AS Touch Project Clock Error
- Enable only non-event system low-power with driven shield
- Touch GUI dock update issue
- RTC count sync issue
- Mutual cap surface XY configuration for XYmuxed devices
- Lump with boost mode
- Touch_example.c file is generated along with touch.c file
- Sleep instruction is moved from touch_process() to touch_example.c file
- MPLAB X IDE v5.50
- MPLAB XC32 C/C++ Compiler v2.50
- MPLAB XIDE plug-ins:
- MPLAB Harmony Configurator (MHC) v3.8.0
- csp v3.9.1
- bsp v3.9.0
- dev_packs v3.9.0
- mhc v3.8.0
- None.
Touch Library v3.9.2 Release
BUG FIXES
- Touch configuration panel cannot open when MHC upgrades to 3.7.0
- Gesture disables timer start
- SAMD5x-E5x driven shield prescaler offset value
- Keys module for boost mode calibration issue
- MPLAB X IDE v5.45
- MPLAB XC32 C/C++ Compiler v2.50
- MPLAB X IDE plug-ins:
- MPLAB Harmony Configurator (MHC) v3.7.0
- csp v3.9.0
- bsp v3.9.0
- dev_packs v3.9.0
- mhc v3.7.0
- None.
Touch Library v3.9.1 Release
BUG FIXES
- Event system low-power support added for SAML2x.
- Project generation for PIC32MZW fixed.
- Updating RTC period value halts the CPU due to count sync. Count sync is disabled.
- Optimzied low-power touch code for one button project.
- MPLAB X IDE v5.45
- MPLAB XC32 C/C++ Compiler v2.50
- MPLAB X IDE plug-ins:
- MPLAB Harmony Configurator (MHC) v3.6.5
- csp v3.8.3
- bsp v3.8.2
- dev_packs v3.8.0
- mhc v3.6.5
- None.
Touch Library v3.9.0 Release
NEW FEATURES SUPPORTED
- Low Power Support extended for - SAMC2x, SAM D1x, SAM E5x, SAM D5x, SAM L2x.
- Driven shield waveform for C2x was not in sync - Corrected.
- Calibration trigger does not automatically trigger corresponding button's calibration in boost mode - Corrected.
- MPLAB X IDE v5.45
- MPLAB XC32 C/C++ Compiler v2.50
- MPLAB X IDE plug-ins:
- MPLAB Harmony Configurator (MHC) v3.6.4
- csp v3.8.3
- bsp v3.8.2
- dev_packs v3.8.0
- mhc v3.6.4
- SAM L2x - Event system based low-power support in later release.
Touch Library v3.8.0 Release
NEW FEATURES SUPPORTED
- Low Power Support
- Lump Support
- Binding Layer is disabled
- MPLAB X IDE v5.40
- MPLAB XC32 C/C++ Compiler v2.41
- MPLAB X IDE plug-ins:
- MPLAB Harmony Configurator (MHC) v3.6.0
- csp v3.8.0
- bsp v3.8.0
- dev_packs v3.8.0
- mhc v3.5.1
- Lump mode mouse drag operation in Touch configurator GUI only operates from top left to bottom right.
Touch Library v3.7.0 Release
NEW DEVICES SUPPORTED
- Device Support for SAM L11.
- Boost mode support (parallel acquisition) added for SAML10 and SAML11 devices.
- Graphical representation of the input clock, available prescaler values, and PTC clock frequencies are displayed in the parameter tab.
- The clock-change warning message, which appears when a new sensor is added, now lists the changes which happen in the background when the user selects Yes.
- The minimum and maximum PTC clock frequency details are added.
- MPLAB X IDE v5.40
- MPLAB XC32 C/C++ Compiler v2.41
- MPLAB X IDE plug-ins:
- MPLAB Harmony Configurator (MHC) v3.5
- csp v3.7.1
- bsp v3.7.0
- dev_packs v3.4.1
- mhc v3.4.0
- none
Touch Library v3.6.0 Release
NEW DEVICES SUPPORTED
- Device Support for SAM HA1
- Device Support for PIC32MZ1025W104132 (HCVD)
- Driven Shield support for SAM D21
- Driven Shield support for SAM DA1
- Driven Shield support for SAM HA1
- Driven Shield support for SAM L2x
- Driven Shield support for SAM C2x
- Driven Shield support for SAM E5x
- Driven Shield support for SAM D51
- Updated the prescaler values in api.h files to include the internal
prescaler division factor.
- For example, in SAML10, the prescaler values from 1, 2, 4, 8 are updated to 4, 8, 16, 32 (to include a fixed internal division factor of 4). Similarly, all prescaler values are updated for all other devices.
- MPLAB X IDE v5.35
- MPLAB XC32 C/C++ Compiler v2.40
- MPLAB X IDE plug-ins:
- MPLAB Harmony Configurator (MHC) v3.4.2
- csp v3.6.1
- bsp v3.6.1
- dev_packs v3.6.1
- mhc v3.3.5
- none
Touch Library v3.5.0 Release
NEW DEVICES SUPPORTEDNEW FEATURES:
- Driven shield support for SAML10 is addded.
- ATSAMDA1 Xplained Pro Mutual Capacitance Example Project with QT1
- ATSAMDA1 Xplained Pro Self Capacitance Example Project with QT1
- ATSAML10 Xplained Pro Driven Shield Example Project with QT7 (updated with Driven Shield)
- ATSAMD10 Xplained Mini Self Capacitance Example Project with onboard Button
- ATSAMD11 Xplained Pro Self Capacitance Example Project with onboard Button
- csp v3.5.0
- bsp v3.5.0
- dev_packs v3.5.0
- mhc v3.3.3
- SAMD10 (C variant) Project generation fails, error is related to clock support.
- MPLAB X IDE v5.25
- MPLAB XC32 C/C++ Compiler v2.30
- MPLAB X IDE plug-ins:
- MPLAB Harmony Configurator (MHC) v3.3.1
Touch Library v3.4.0 Release
NEW DEVICES SUPPORTEDNEW FEATURES:NEW DEMO PROJECTS:
- ATSAML21 Xplained Pro Mutual Capacitance Example Project with QT1
- ATSAML21 Xplained Pro Self Capacitance Example Project with onboard Button
- ATSAML22 Xplained Pro Mutual Capacitance Example Project with QT1
- ATSAML22 Xplained Pro Self Capacitance Example Project with onboard Button
- ATSAML10 Xplained Pro Self Capacitance Example Project with QT7
- csp v3.4.0
- bsp v3.4.0
- dev_packs v3.3.0
- mhc v3.3.0.1
- Clock configuration set by touch configurator is removed when touch configurator is closed. This bug is fixed.
- MPLAB X IDE v5.20
- MPLAB XC32 C/C++ Compiler v2.20
- MPLAB X IDE plug-ins:
- MPLAB Harmony Configurator (MHC) v3.3.1
Touch Library v3.3.0 Release
NEW FEATURES
- Touch Surface (One Finger and Two Fingers) and Gesture firmware, GUI along with DataVisualizer and 2D Touch Surface Utility (Kronocomm) support for SAMC2x, SAMD2x, SAMD51, SAME51, SAME53, SAME54 devices.
- Clock selection support for proper operation of Touch, automated through the Touch configurator.
- csp v3.4.0
- bsp v3.4.0
- dev_packs v3.4.0
- mhc v3.3.1
- Scroller + Surface combination is not supported.
- MPLAB X IDE v5.20
- MPLAB XC32 C/C++ Compiler v2.20
- MPLAB X IDE plug-ins:
- MPLAB Harmony Configurator (MHC) v3.3.1
Touch Library v3.2.0 Release
NEW DEVICES SUPPORTEDNEW FEATURES
- Slider and Wheel Firmware Support along with GUI Support
- Support for Tabbed View of Data-Visualizer Software
- ATSAMD20 Xplained Pro Mutual Capacitance Example Project with QT1
- ATSAMD20 Xplained Pro Self Capacitance Example Project with QT1
- ATSAMD21 Xplained Pro Mutual Capacitance Example Project with QT1
- ATSAMD21 Xplained Pro Self Capacitance Example Project with QT1
- ATSAME54 Xplained Pro Mutual Capacitance Example Project with QT1
- ATSAME54 Xplained Pro Self Capacitance On Board Example Project
- ATSAMC21 Xplained Pro Mutual Capacitance Example Project with QT1
- ATSAMC21 Xplained Pro Self Capacitance Example Project with QT1
- csp v3.3.0
- bsp v3.3.0
- dev_packs v3.3.0
- mhc v3.3.0.1
- Touch libraries are built with v2.15 compiler version. Touch Applications may not work properly with other compiler versions.
- MPLAB X IDE v5.20
- MPLAB XC32 C/C++ Compiler v2.15
- MPLAB X IDE plug-ins:
- MPLAB Harmony Configurator (MHC) v3.3.0.1
Touch Library v3.1.1 Release
BUG FIX
- Compilation error related to Data Visualizer code when Frequency Hop is NOT enabled.
- csp v3.2.0
- dev_packs v3.2.0
- mhc v3.2.0
- MPLAB X IDE v5.15
- MPLAB XC32 C/C++ Compiler v2.15
- MPLAB X IDE plug-ins:
- MPLAB Harmony Configurator (MHC) v3.2.0.
Touch Library v3.1.0 Release
NEW FEATURES
- Button only touch support for SAM C2x device family along with Data Visualizer option
- Touch configurator GUI
- ATSAMC21 Xplained Pro Mutual Capacitance Example Project with QT1
- ATSAMC21 Xplained Pro Self Capacitance Example Project with QT1
- csp v3.2.0
- dev_packs v3.2.0
- mhc v3.2.0
- None.
- MPLAB X IDE v5.15
- MPLAB XC32 C/C++ Compiler v2.15
- MPLAB X IDE plug-ins:
- MPLAB Harmony Configurator (MHC) v3.2.0.