47.8.12 MCSPI Chip Select Register

This register can only be written if the WPEN bit is cleared in the MCSPI Write Protection Mode Register.

Note: MCSPI_CSRx must be written even if default reset values will be used. The BITS field is not updated with the translated value unless the register is written.
Name: MCSPI_CSRx
Offset: 0x30 + x*0x04 [x=0..3]
Reset: 0x00000000
Property: Read/Write

Bit 3130292827262524 
 DLYBCT[7:0] 
Access R/WR/WR/WR/WR/WR/WR/WR/W 
Reset 00000000 
Bit 2322212019181716 
 DLYBS[7:0] 
Access R/WR/WR/WR/WR/WR/WR/WR/W 
Reset 00000000 
Bit 15141312111098 
 SCBR[7:0] 
Access R/WR/WR/WR/WR/WR/WR/WR/W 
Reset 00000000 
Bit 76543210 
 BITS[3:0]CSAATCSNAATNCPHACPOL 
Access R/WR/WR/WR/WR/WR/WR/WR/W 
Reset 00000000 

Bits 31:24 – DLYBCT[7:0] Delay Between Consecutive Transfers

This field defines the delay between two consecutive transfers with the same peripheral without removing the chip select. The delay is always inserted after each transfer and before removing the chip select if needed.

When DLYBCT = 0, no delay between consecutive transfers is inserted and the clock keeps its duty cycle over the character transfers.

Otherwise, the following equations determine the delay:

If MCSPI_MR.BRSRCCLK = 0: DLYBCT = Delay Between Consecutive Transfers × fperipheral clock / 32

If MCSPI_MR.BRSRCCLK = 1: DLYBCT = Delay Between Consecutive Transfers × fGCLK / 32

Bits 23:16 – DLYBS[7:0] Delay Before SPCK

This field defines the delay from NPCS falling edge (activation) to the first valid SPCK transition.

When DLYBS = 0, the delay is half the SPCK clock period.

Otherwise, the following equations determine the delay:

If MCSPI_MR.BRSRCCLK = 0: DLYBS = Delay Before SPCK × fperipheral clock

If MCSPI_MR.BRSRCCLK = 1: DLYBS = Delay Before SPCK × fGCLK

Bits 15:8 – SCBR[7:0] Serial Clock Bit Rate

In Host mode, the MCSPI Interface uses a modulus counter to derive the SPCK bit rate from the clock defined by the MCSPI_MR.BRSRCCLK bit. The bit rate is selected by writing a value from 1 to 255 in the SCBR field. The following equations determine the SPCK bit rate:

If MCSPI_MR.BRSRCCLK = 0: SCBR = fperipheral clock / SPCK Bit Rate

If MCSPI_MR.BRSRCCLK = 1: SCBR = fGCLK / SPCK Bit Rate

Programming the SCBR field to 0 is forbidden. Triggering a transfer while SCBR is at 0 can lead to unpredictable results.

If MCSPI_MR.BRSRCCLK = 1, SCBR must be programmed with a value greater than 1.

At reset, SCBR is 0 and the user has to program it at a valid value before performing the first transfer.

Note: If one of the MCSPI_CSRx.SCBR fields is set to 1, the other MCSPI_CSRx.SCBR fields must be set to 1 as well, if they are used to transfer data. If they are not used to transfer data, they can be set to any value.

Bits 7:4 – BITS[3:0] Bits Per Transfer

See Note above.

The BITS field determines the number of data bits transferred. Reserved values should not be used.

ValueNameDescription
0 8_BIT

8 bits for transfer

1 9_BIT

9 bits for transfer

2 10_BIT

10 bits for transfer

3 11_BIT

11 bits for transfer

4 12_BIT

12 bits for transfer

5 13_BIT

13 bits for transfer

6 14_BIT

14 bits for transfer

7 15_BIT

15 bits for transfer

8 16_BIT

16 bits for transfer

9 –

Reserved

10 –

Reserved

11 –

Reserved

12 –

Reserved

13 –

Reserved

14 –

Reserved

15 –

Reserved

Bit 3 – CSAAT Chip Select Active After Transfer

ValueDescription
0

The peripheral chip select line rises as soon as the last transfer is achieved.

1

The peripheral chip select line does not rise after the last transfer is achieved. It remains active until a new transfer is requested on a different chip select.

Bit 2 – CSNAAT Chip Select Not Active After Transfer (ignored if CSAAT = 1)

ValueDescription
0

The peripheral chip select line does not rise between two transfers if MCSPI_TDR is reloaded before the end of the first transfer and if the two transfers occur on the same chip select.

1

The peripheral chip select line rises systematically after each transfer performed on the same client. It remains inactive after the end of transfer for a minimal duration of:

If MCSPI_MR.BRSRCCLK = 0:

DLYBCS f peripheral clock

If MCSPI_MR.BRSRCCLK = 1:

DLYBCS f GCLK

If field DLYBCS is lower than 6, a minimum of six periods is introduced.

Bit 1 – NCPHA Clock Phase

NCPHA determines which edge of SPCK causes data to change and which edge causes data to be captured. NCPHA is used with CPOL to produce the required clock/data relationship between host and client devices.

ValueDescription
0

Data is changed on the leading edge of SPCK and captured on the following edge of SPCK.

1

Data is captured on the leading edge of SPCK and changed on the following edge of SPCK.

Bit 0 – CPOL Clock Polarity

CPOL is used to determine the inactive state value of the serial clock (SPCK). It is used with NCPHA to produce the required clock/data relationship between host and client devices.

ValueDescription
0

The inactive state value of SPCK is logic level zero.

1

The inactive state value of SPCK is logic level one.