2.13 Build and Program
The demo project will be compiled and programmed to PIC32CXMTG-EK board.
Build the application
- Open the project Properties by Right Clicking on the project name (MyFirstG3app)
- Make sure that XC32 compiler toolchain is selected. Press OK
Figure . Select Compiler 
- Build the application by clicking on the Build Main Project or Clean and Build Main Project menu command
Figure . Build Project 
- Verify the build is SUCCESSFUL in Output window
Figure . Successful Build 
Program the application
- Connect a micro-USB cable from computer to the USB port on the PIC32CXMTG-EK board
- Click on Make and Program Device Main Project menu command
Figure . Make And Program Device 
- If not already done, select the programming tool for the connected board
Figure . Select Programming Tool 
At this point we have a G3 Device running on the PIC32CXMTG-EK board. It can be tested against one of the G3 Coordinator examples available in smartenergy_g3_apps repository.