4 Installing the Library
The following instructions describe how to install the MCC plugin and the I2C Simple Driver in MPLAB X IDE.
To install the MPLAB® Code Configurator Plugin:
- In MPLAB X IDE, select Plugins from the Tools menu.
- Select the Available Plugins tab.
- Check the box for the MPLAB® Code Configurator and click on Install.
To install the Melody I2C Simple Driver:
- Open MCC in MPLAB® X
- In the Content Type window, select MCC Melody
- Under Optional Content, go to Optional Content → Drivers
- Tick the box next to I2CSIMPLE and click Finish
- In the Content Manager window, select the latest version or the preferred version of the Library and click Apply.