3 EEPROM Operation Command and EEPROM Operation Event
The EEPROM operation command is packed into the HCI command packet, and the E2PROM operation event is packed into the HCI event packet. For more details, see the following table from Bluetooth Core Specification v5.2 (Core_v5.2).
| HCI Packet Type | HCI Packet Indicator |
|---|---|
| HCI command packet | 0x01 |
| HCI ACL data packet | 0x02 |
| HCI synchronous data packet | 0x03 |
| HCI event packet | 0x04 |
| HCI ISO data packet | 0x05 |
The EEPROM command packet always starts with 0x01. The following figure illustrates the rest of the HCI command from the Core_v5.2. The OpCode has a 16-bit length, where the OpCode Command Field (OCF) combines each OpCode in the lower 10 bits and the OpCode Group Field (OGF) in the upper 6 bits.
The EEPROM event packet always starts with 0x04. The following figure illustrates the E2PROM event = 0x04, along with the rest of the HCI event packet from the Core_v5.2.
The EEPROM event is packed in the HCI_Command_Complete event with the event code
set to 0x0E. For more details, refer to Section 7.7.14 from the Bluetooth Core Specification v5.2.
| Event | Event Code | Event Parameters |
|---|---|---|
HCI_Command_Complete | 0x0E |
|