1.19 PWM Generation

This example shows how to use the PWM peripheral to generate 3-phase PWM signals with dead time.

Description

This example shows how to configure the PWM to generate synchronous 3-phase PWM signals with dead time (used for motor control). The duty cycle of the PWM is updated in the interrupt handler.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/pwm/pwm_synchronous_channels/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project Name Description
sam_a7g5_ek.X MPLABX project for SAMA7G54 Evaluation Kit

Setting Up AT91Bootstrap Loader

To load the application binary onto the target device, we need to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project Name Description
sam_a7g5_ek.X SAMA7G54 Evaluation Kit

Setting Up SAMA7G5 Evaluation Kit

SETTING UP THE BOARD
  • Connect the Debug USB port on the board to the computer using a micro USB cable

Running the Application

  1. Build and Program the application using their respective IDEs
  2. Observe the high-side and low-side PWM waveforms on the oscilloscope
  3. Observe the dead time between the high side and low side
Refer to the below table for PWM output pins for different boards:
PWM Channel SAMA7G5 Evaluation Kit
CH0_PWML PE02 (Pin 32 of RPi connector(J13))
CH0_PWMH PE03 (Pin 38 of RPi connector(J13))
CH1_PWML PE04 (Pin 35 of RPi connector(J13))
CH1_PWMH PE05 (Pin 40 of RPi connector(J13))
CH2_PWML PE06 (Pin 12 of RPi connector(J13))
CH2_PWMH PE07 (Pin 11 of RPi connector(J13))