1.5 OTA Bootloader Host Script Help

The following python scripts are used in order to update the application binary image

  1. ota_host_mcu_header.py - This script will add the OTA Host MCU Header to the application binary and image.bin will be generated as intermediate output binary image. Path of the tool within the bootloader application repository is tools/ota_host_mcu_header.py

  2. ota_rnbd_header.py - This script will add the OTA RNBD Header to the image.bin intermediate binary and it generates RNBD_image.bin application binary as final output binary image. Path of the tool within the bootloader application repository is tools/ota_rnbd_header.py

The following steps to be performed to update the application binary image

Step 1: Run ota_host_mcu_header.py script. Below is the syntax to show help menu for the script

python <harmony3_repo_path>/tools/ota_host_mcu_header.py --help

Below syntax and example

ota_host_mcu_header

Description

  • It should be used with -p (--programAddr) option to specify Flash Application Program Address
  • It should be used with -j (--jumpAddr) option to specify Flash Application Execution Address
  • It should be used with -f (--binary) option to specify binary input file
  • In case of external memory only, It should be used with -l (--loadAddr) option to specify External Memory Program Address

Dual Bank:

python <harmony3_repo_path>/tools/ota_host_mcu_header.py -p 0x82000 -j 0x2000 -f sam_e54_xpro.X.production.bin

External Memory:

python <harmony3_repo_path>/tools/ota_host_mcu_header.py -p 0x402000 -j 0x402000 -l 0x0 -f sam_e70_xult.X.production.bin

Step 2: Run ota_rnbd_header.py script. Below is the syntax to show help menu for the script

python <harmony3_path>/bootloader_apps_ota/tools/ota_rnbd_header.py --help

Below syntax and example

ota_rnbd_header

Description

  • It should be used with -f (--binary) option to specify binary input file

Dual Bank/External Memory:

python <harmony3_path>/bootloader_apps_ota/tools/ota_rnbd_header.py -f image.bin

Once command is executed successfully then it generates RNBD_image.bin final application binary image

For Cortex-M based Dual Bank Devices

  • User can generate an additional inactive bank bootloader hex file through post build command in the OTA bootloader project. The hex_merge python script can be used to combine unified HEX file (for Bootloader and application in active bank) and bootloader inactive bank HEX file (for Bootloader in inactive bank)
python hex_merge.py --help

Below syntax and example

hex_merge

Description

  • It should be used with -o (--hexfile1) option to specify an unified HEX file (for Bootloader and application in active bank)
  • It should be used with -a (--hexfile2) option to specify a bootloader inactive bank HEX file
python <harmony3_path>/bootloader_apps_ota/tools/hex_merge.py -o sam_e54_xpro.X.production.unified.hex -a sam_e54_xpro.X.production_inactive_bank.hex

Once command is executed successfully then sam_e54_xpro.X.production.unified.hex is updated and it contains bootloader inactive bank hex file along with active bank bootloader hex file and active bank application hex file