22.3.3.1 Register Synchronization Categories

Most of the I/O registers need to be synchronized to the TCD core clock domain. This is done differently for different register categories.

Table 22-2. Categorization of Registers
Enable and Command RegistersDouble-Buffered RegistersStatic RegistersRead-Only RegistersNormal I/O Registers
TCDn.CTRLA (ENABLE bit)TCDn.DLYCTRLTCDn.CTRLA(1) (All bits except ENABLE bit)TCDn.STATUSTCDn.INTCTRL
TCDn.CTRLETCDn.DLYVALTCDn.CTRLBTCDn.CAPTUREATCDn.INTFLAGS
TCDn.DITCTRLTCDn.CTRLCTCDn.CAPTUREB
TCDn.DITVALTCDn.CTRLD
TCDn.DBGCTRLTCDn.EVCTRLA
TCDn.CMPASETTCDn.EVCTRLB
TCDn.CMPACLRTCDn.INPUTCTRLA
TCDn.CMPBSETTCDn.INPUTCTRLB
TCDn.CMPBCLRTCDn.FAULTCTRL(2)
Note:
  1. The bits in the Control A (TCDn.CTRLA) register are enable-protected, except the ENABLE bit. They can only be written when ENABLE is written to ‘0’ first.
  2. This register is protected by the Configuration Change Protection Mechanism, requiring a timed write procedure for changing its value settings.

Enable and Command Registers

Because of the synchronization between the clock domains, it is only possible to change the ENABLE bit in the Control A (TCDn.CTRLA) register, while the Enable Ready (ENRDY) bit in the Status (TCDn.STATUS) register is ‘1’.

The Control E (TCDn.CTRLE) register is automatically synchronized to the TCD core domain when the TCD is enabled and as long as no synchronization is ongoing already. Check if the Command Ready (CCMDRDY) bit in TCDn.STATUS is ‘1’ to ensure that it is possible to issue a new command. TCDn.CTRLE is a strobe register that will clear itself when the command is sent.

Double-Buffered Registers

The double-buffered registers can be updated in normal I/O writes, while TCD is enabled and no synchronization between the two clock domains is ongoing. Check that the CMDRDY bit in TCDn.STATUS is ‘1’ to ensure that it is possible to update the double-buffered registers. The values will be synchronized to the TCD core domain when a synchronization command is sent or when TCD is enabled.

Table 22-3. Issuing Synchronization Command
Synchronization Issuing BitDouble Register Update
CTRLC.AUPDATEEvery time the CMPBCLRH register is written, the synchronization occurs at the end of the TCD cycle.
CTRLE.SYNC (1)Occurs once, as soon as the SYNC bit is synchronized with the TDC domain.
CTRLE.SYNCEOC (1)Occurs once at the end of the next TCD cycle.
Note:
  1. If synchronization is already ongoing, the action has no effect.

Static Registers

Static registers cannot be updated while TCD is enabled. Therefore, these registers must be configured before enabling TCD. To see if TCD is enabled, check if ENABLE in TCDn.CTRLA is read as ‘1’.

Normal I/O and Read-Only Registers

Normal I/O and read-only registers are not constrained by any synchronization between the domains. The read-only registers inform about synchronization status and values synchronized from the core domain.