1.1.4 PIC32MK MCJ Curiosity Pro: Building and Running the UART Bootloader applications

Downloading and building the application

To clone or download this application from Github,go to the main page of this repository and then click Clone button to clone this repo or download as zip file. This content can also be download using content manager by following these instructions

Path of the application within the repository is apps/uart_bootloader/

To build the application, refer to the following table and open the project using its IDE.

Bootloader Application

Project NameDescription
bootloader/firmware/pic32mk_mcj_curiosity_pro.XMPLABX Project for PIC32MK MCJ Curiosity Pro

Test Application

Project NameDescription
test_app/firmware/pic32mk_mcj_curiosity_pro.XMPLABX Project for PIC32MK MCJ Curiosity Pro

Setting up PIC32MK MCJ Curiosity Pro

  • Connect micro USB cable to the 'Debug USB' connector(J1) on the board to the computer

Setting up the host script

Running the Application

  1. Open the test application project test_app/firmware/pic32mk_mcj_curiosity_pro.X in the IDE

  2. Build the project to generate the binary (Do not program the binary)

  3. Open the bootloader project bootloader/firmware/pic32mk_mcj_curiosity_pro.X in the IDE

  4. Build and program the application using the IDE

  5. Run the btl_host.py from command prompt to program the application binary

     python <harmony3_path>/bootloader/tools/btl_host.py -v -i <COM PORT> -d pic32mk -a 0x9D000000 -f <harmony3_path>/bootloader_apps_uart/apps/uart_bootloader/test_app/firmware/pic32mk_mcj_curiosity_pro.X/dist/pic32mk_mcj_curiosity_pro/production/pic32mk_mcj_curiosity_pro.X.production.bin
  6. Following snapshot shows output of successfully programming the test application

    • Rebooting and Reboot Done messages in below output signifies that bootloading is successful
    output
  7. If above step is successful then the LED2 should start blinking

  8. Open the Terminal application (Ex.:Tera Term) on the computer

  9. Configure the serial port settings as follows:

    • Baud : 115200
    • Data : 8 Bits
    • Parity : None
    • Stop : 1 Bit
    • Flow Control : None
  10. Reset or Power cycle the device

  11. LED2 should start blinking and you should see below output on the console

    output
  12. Press and hold the Switch SW200 to trigger Bootloader from test application and you should see below output

    output
  13. Repeat Steps 5-11 once and jump to Step-14.

    • This step is to verify that bootloader is running after triggering bootloader from test application in Step 12
  14. Press and hold the Switch SW200 and then press Reset button or Power cycle the device to force trigger bootloader at startup

  15. Repeat Steps 5-11 once

    • This step is to verify whether bootloader is triggered by switch press at reset

Additional Steps (Optional)