6 Relevant Links
The following tables contain links to the most relevant documents and software for the AVR-IoT Wx Development Boards. For those accessing the electronic version of this document, the active links below will redirect to the appropriate website.
| URL | Description | |
|---|---|---|
| AVR-IoT WG website | www.microchip.com/DevelopmentTools/ProductDetails.aspx?PartNO=AC164160 | Find schematics, design files, and purchase the board. Set up for Google Cloud IoT Core |
| AVR-IoT WG on MCHPDirect | www.microchipdirect.com/ProductSearch.aspx?Keywords=AC164160 | Purchase the AVR-IoT WG board on Microchip Direct |
| AVR-IoT WA website | www.microchip.com/DevelopmentTools/ProductDetails.aspx?PartNO=EV15R70A | Find schematics, design files, and purchase the board. Set up for Amazon Web Services |
| AVR-IoT WA on MCHPDirect | www.microchipdirect.com/ProductSearch.aspx?Keywords=EV15R70A | Purchase the AVR-IoT WA board on Microchip Direct |
| AVR-IoT Wx Hardware User Guide | microchip.com/DS50002805 | Find more information on the hardware of the AVR-IoT Wx boards. |
| AVR-IoT WG for MPLAB X on GitHub | Source code.hex file | Download the AVR-IoT WG source code and .hex files for MPLAB X from GitHub |
| AVR-IoT WG for Atmel Studio on GitHub | Source code.hex file | Download the AVR-IoT WG source code and .hex files for Atmel Studio from GitHub |
| AVR-IoT WA for MPLAB X on GitHub | Source code.hex file | Download the AVR-IoT WA source code and .hex files for MPLAB X from GitHub |
| AVR-IoT WA for Atmel Studio on GitHub | Source code.hex file | Download the AVR-IoT WA source code and .hex files for Atmel Studio from Gitb |
| URL | Description | |
|---|---|---|
| MPLAB X IDE | www.microchip.com/mplab/mplab-x-ide | Free IDE to develop applications for Microchip microcontrollers and digital signal controllers. |
| Atmel Studio | www.microchip.com/development-tools/atmel-studio-7 | Free IDE for the development of C/C++ and assembler code for microcontrollers. |
| MPLAB Code Configurator (MCC) | www.microchip.com/mplab/mplab-code-configurator | Free, graphical programming environment that generates seamless, easy-to-understand C code to be inserted into the project. Using an intuitive interface, it enables and configures a rich set of peripherals and functions specific to the application. |
| Atmel START | www.microchip.com/start | Online tool that helps the user to select and configure software components and tailor the embedded application in a usable and optimized manner. |
| Microchip Sample Store | www.microchip.com/samples/default.aspx | Microchip sample store where the user can order samples of devices. |
| Data Visualizer | www.microchip.com/mplab/avr-support/data-visualizer | A program used for processing and visualizing data. The Data Visualizer can receive data from various sources such as the Embedded Debugger Data Gateway Interface found on Xplained Pro boards and COM ports. |