Introduction
This application note offers a comprehensive guide on programming the ATA8510-EK1 application demonstrator using the built-in hardware, eliminating the need for an additional programming tool. This method enhances the user experience by incorporating the ATA Evaluation Graphical User Interface (GUI). The use of the GUI not only simplifies the programming process but also provides the user with practical knowledge and hands-on experience with the tool, significantly improving their understanding and skill set for future projects.