2 Revision History
The following is a list of changes by version to this document.
Note: Some revision letters are not used - the letters
I and O - as they can be confused for numbers in
some fonts.Revision B (April 2023)
- 1. CI/CD Wizard: MPLAB ICD 5 added as hardware tool with network support.
- 1.3.1.4 Testing Tools and 1.3.2.9 CI/CD Wizard Output: Sections made more generic with reference to supported hardware tools.
- 1.3.2.6 CI/CD Wizard Dialog 6: Dialog updated to allow selection of MPLAB ICE 4 or MPLAB ICD 5.
- 1.5.2.2 Step 2. Connect MPLAB ICE 4 to Target: Title updated to remove “Using the Breakout Board” and section updated to add information on using the high-speed cable to connect to the target as well. Updated Table 1-1. “Connection Summary.”
- 1.5.3 Running Unit Tests on MPLAB ICD 5: Section added to describe how to use MPLAB ICD 5 to run Unity tests.
Revision A (December 2021)
Initial release of this document.