| AP_VER=Algorithm Plugin
Version. |
| AREAS_TO_PROGRAM=The following
memory area(s) will be programmed: |
| AREAS_TO_READ=The following
memory area(s) will be read: |
| AREAS_TO_VERIFY=The following
memory area(s) will be verified: |
| BLANK_CHECK_COMPLETE=Blank
check complete, device is blank. |
| BLANK_CHECKING=Blank
Checking... |
| BOOT_CONFIG_MEMORY=boot config
memory. |
| BOOT_VER=Boot Version. |
| BOOTFLASH=boot flash. |
| BP_CANT_B_DELETED_WHEN_RUNNING=software breakpoints cannot be removed
while the target is running. The selected breakpoint will be removed the
next time the target halts. |
| CANT_CREATE_CONTROLLER=Unable
to find the tool controller class. |
| CANT_FIND_FILE=Unable to locate
file %s. |
| CANT_OP_BELOW_LVPTHRESH=The
voltage level selected %f, is below the minimum erase voltage of %f. The
operation cannot continue at this voltage level. |
| CANT_PRESERVE_PGM_MEM=Unable
to preserve program memory: Invalid range Start = %08x, End =
%08x. |
| CANT_READ_REGISTERS=Unable to
read target register(s). |
| CANT_READ_SERIALNUM=Unable to
read the device serial number. |
| CANT_REMOVE_SWPS_BUSY=The ICD
4 is currently busy and cannot remove software breakpoints at this time.
|
| CHECK_4_HIGH_VOLTAGE_VPP=CAUTION: Check that the device selected in
MPLAB IDE (%s) is the same one that is physically attached to the debug
tool. Selecting a 5V device when a 3.3V device is connected can result
in damage to the device when the debugger checks the device ID. Do you
wish to continue? |
| CHECK_PGM_SPEED=You have set
the program speed to %s. The circuit on your board may require you to
slow the speed down. Please change the setting in the tool properties to
low and try the operation again. |
| COMM_PROTOCOL_ERROR=A
communication error with the debug tool has occurred. The tool will be
reset and should re-enumerate shortly. |
| COMMAND_TIME_OUT=ICD 4 has
timeout out waiting for a response to command %02x. |
| CONFIGURATION=configuration. |
| CONFIGURATION_MEMORY=configuration memory. |
| CONNECTION_FAILED=Connection
Failed. |
| CORRUPTED_STREAMING_DATA=Invalid streaming data has been detected. Run
time watch or trace data may no longer be valid. It is recommended that
you restart your debug session. |
| CPM_TO_TARGET_FAILED=An
exception occurred during ControlPointMediator.ToTarget(). |
| DATA_FLASH_MEMORY=Data Flash
memory. |
| DATA_FLASH=data flash. |
| DEBUG_INFO_PGM_FAILED=Could
not enter debug mode because programming the debug information failed.
Invalid combinations of config bits may cause this problem. |
| DEBUG_READ_INFO=Reading the
device while in debug mode may take a long time due to the target
oscillator speed. Reducing the range that you'd like to read (under the
ICD 4 project properties) can mitigate the situation. The abort
operation can be used to terminate the read operation if necessary.
|
| DEVICE_ID_REVISION=Device Id
Revision. |
| DEVICE_ID=Device Id. |
| DEVID_MISMATCH=Target Device ID
(0x%x) is an Invalid Device ID. Please check your connections to the
Target Device. |
| DISCONNECT_WHILE_BUSY=The tool
was disconnected while it was busy. |
| EEDATA_MEMORY=EEData
memory. |
| EEDATA=EEData. |
| EMULATION_MEMORY_READ_WRITE_ERROR=An error occurred while trying to
read/write MPLAB's emulation memory: Address=%08x. |
| END=end. |
| ENSURE_SELF_TEST_READY=Please
ensure the RJ-11 cable is connected to the test board before
continuing. |
| ENSURE_SELF_TEST_READY=Please
ensure the RJ-11 cable is connected to the test board before continuing.
Would you like to continue? |
| ENV_ID_GROUP=Device
Identification. |
| ERASE_COMPLETE=Erase
successful. |
| ERASING=Erasing... |
| FAILED_2_PGM_DEVICE=Failed to
program device. |
| FAILED_CREATING_COM=Unable
create communications object (RI4Com). |
| FAILED_CREATING_DEBUGGER_MODULES=Initialization failed: Failed creating
the debugger module. |
| FAILED_ESTABLISHING_COMMUNICATION=Unable to establish tool
communications. |
| FAILED_GETTING_DBG_EXEC=A
problem occurred while trying to load the debug executive. |
| FAILED_GETTING_DEVICE_INFO=Initialization failed: Failed while
retrieving device database (.pic) information. |
| FAILED_GETTING_EMU_INFO=Initialization failed: Failed getting emulation
database information. |
| FAILED_GETTING_PGM_EXEC=A
problem occurred while trying to load the program executive. |
| FAILED_GETTING_TEX=Unable to
obtain the ToolExecMediator. |
| FAILED_GETTING_TOOL_INFO=Initialization failed: Failed while retrieving
tool database (.ri4) information. |
| FAILED_INITING_DATABASE=Initialization failed: Unable to initialize the
too database object. |
| FAILED_INITING_DEBUGHANDLER=Initialization failed: Unable to initialize
the DebugHandler object. |
| FAILED_PARSING_FILE=Failed to
parse firmware file: %s. |
| FAILED_READING_EMULATION_REGS=Failed to read emulation memory. |
| FAILED_READING_MPLAB_MEMORY=Unable to read %s memory from %0x08 to
%0x08. |
| FAILED_SETTING_SHADOWS=Failed
to properly set shadow registers. |
| FAILED_SETTING_XMIT_EVENTS=Unable to synchronize run time data
semiphores. |
| FAILED_STEPPING=Failed while
stepping the target. |
| FAILED_TO_GET_DEVID=Failed to
get Device ID. Please make sure the target device is attached and try
the operation again. |
| FAILED_TO_INIT_TOOL=Failed to
initialize ICD 4. |
| FAILED_UPDATING_BP=Failed to
update breakpoint:\nFile: %s\naddress: %08x. |
| FAILED_UPDATING_FIRMWARE=Failed to properly update the
firmware. |
| FILE_REGISTER=file
register. |
| FIRMWARE_DOWNLOAD_TIMEOUT=ICD
4 timeout out during the firmware download process. |
| FLASH_DATA_MEMORY=Flash data
memory. |
| FLASH_DATA=flash data. |
| FPGA_VER=FPGA Version. |
| FRCINDEBUG_NEEDS_CLOCKSWITCHING=To use FRC in debug mode the clock
switching configuration bits setting must be enabled. Please enable
clock switching and retry the requested operation. |
| FW_DOESNT_SUPPORT_DYNBP=The
current ICD 4 firmware does not support setting run time breakpoints for
the selected device. Please download firmware version %02x.%02x.%02x or
higher. |
| GOOD_ID_MISMATCH=Target Device
ID (0x%x) is a valid Device ID but does not match the expected Device ID
(0x%x) as selected. |
| HALTING=Halting... |
| HIGH=High. |
| HOLDMCLR_FAILED=Hold in reset
failed. |
| IDS_SELF_TEST_BOARD_PASSED=ICD4 is functioning properly. If you are
still having problems with your target circuit please check the Target
Board Considerations section of the online help. |
| IDS_ST_CLKREAD_ERR=Test
interface PGC clock line read failure. |
| IDS_ST_CLKREAD_NO_TEST=Test
interface PGC clock line read not tested. |
| IDS_ST_CLKREAD_SUCCESS=Test
interface PGC clock line read succeeded. |
| IDS_ST_CLKWRITE_ERR=Test
interface PGC clock line write failure. Please ensure that the tester is
properly connected. |
| IDS_ST_CLKWRITE_NO_TEST=Test
interface PGC clock line write not tested. |
| IDS_ST_CLKWRITE_SUCCESS=Test
interface PGC clock line write succeeded. |
| IDS_ST_DATREAD_ERR=Test
interface PGD data line read failure. |
| IDS_ST_DATREAD_NO_TEST=Test
interface PGD data line read not tested. |
| IDS_ST_DATREAD_SUCCESS=Test
interface PGD data line read succeeded. |
| IDS_ST_DATWRITE_ERR=Test
interface PGD data line write failure. |
| IDS_ST_DATWRITE_NO_TEST=Test
interface PGD data line write not tested. |
| IDS_ST_DATWRITE_SUCCESS=Test
interface PGD data line write succeeded. |
| IDS_ST_LVP_ERR=Test interface
LVP control line failure. |
| IDS_ST_LVP_NO_TEST=Test
interface LVP control line not tested. |
| IDS_ST_LVP_SUCCESS=Test
interface LVP control line test succeeded. |
| IDS_ST_MCLR_ERR=Test interface
MCLR level failure. |
| IDS_ST_MCLR_NO_TEST=Test
interface MCLR level not tested. |
| IDS_ST_MCLR_SUCCESS=Test
interface MCLR level test succeeded. |
| IDS_TEST_NOT_COMPLETED=Interface test could not be completed. Please
contact your local FAE/CAE to SAR the unit. |
| INCOMPATIBLE_FW=The REAL ICE
firmware in not compatible with the current version of MPLAB X
software. |
| INVALID_ADDRESS=The operation
cannot proceed because the %s address is outside the devices address
range of 0x%08x - 0x%08x. |
| MEM_RANGE_ERROR_BAD_END_ADDR=Invalid program range end address %s
received. Please check the manual program ranges on the debug tool's,
"Memories to Program" property page. |
| MEM_RANGE_ERROR_BAD_START_ADDR=Invalid program range start address %s
received. Please check the manual program ranges on the debug tool's,
"Memories to Program" property page. |
| MEM_RANGE_ERROR_END_LESSTHAN_START=Invalid program range received: end
address %s < start address %s. Please check the manual program ranges
on the debug tool's, "Memories to Program" property page. |
| MEM_RANGE_ERROR_ENDADDR_NOT_ALIGNED=Invalid program range received: end
address %s is not aligned on a proper 0x%x address boundary. Please
check the manual program ranges on the debug tool's, "Memories to
Program" property page. |
| MEM_RANGE_ERROR_STARTADDR_NOT_ALIGNED=Invalid program range received:
start address %s is not aligned on a proper 0x%x address boundary.
Please check the manual program ranges on the debug tool's, "Memories to
Program" property page. |
| MEM_RANGE_ERROR_UNKNOWN=An
unknown error has occurred while trying to validate the user entered
memory ranges. |
| MEM_RANGE_ERROR_WRONG_DATABASE=Unable to access data object while
validating user entered memory ranges. |
| MEM_RANGE_OUT_OF_BOUNDS=The
selected program range, %s, does not fall within the proper range for
the memory area selected. Please check the manual program ranges on the
debug tool's, "Memories to Program" property page. |
| MEM_RANGE_STRING_MALFORMED=The
memory range(s) entered on the, "Memories to Program" property page (%s)
is not formatted properly. |
| MISSING_BOOT_CONFIG_PARAMETER=Unable to find boot config start/end
address in database. |
| MUST_SET_LVPBIT_WITH_LVP=The
low voltage programming feature requires the LVP configuration bit to be
enabled on the target device. Please enable this configuration bit and
try the operation again. |
| NEW_FIRMWARE=Now Downloading
new Firmware for target device: %s |
| NMMR=NMMR |
| NO_DYNAMIC_BP_SUPPORT_AT_ALL=The current device does not support the
ability to set breakpoints while the devices is running. The breakpoint
will be applied prior to the next time you run the device. |
| NO_PGM_HANDLER=Cannot program
software breakpoints. The program handler has not been
initialized. |
| NORMAL=Normal. |
| OP_FAILED_FROM_CP=The requested
operation failed because the device is code protected. |
| OpenIDE-Module-Name=ICD
4 |
| OPERATION_NOT_SUPPORTED=This
operation is not supported for the selected device. |
| OUTPUTWIN_TITLE=ICD 4. |
| PERIPHERAL=Peripheral. |
| POWER_ERROR_NO_9V=The
configuration is set for the tool to provide power to the target but the
9V power jack is not detected. Please ensure the external 9V barrel jack
is connected to the tool. |
| POWER_ERROR_NO_POWER_SRC=The
configuration is set for the target board to supply its own power but no
voltage has been detected on VDD. Please ensure you have your target
powered up and try again. |
| POWER_ERROR_POWER_SRC_CONFLICT=The configuration is set for the tool to
provide power to the target but there is voltage already detected on
VDD. This is a conflict. Please ensure your target is not supplying
voltage to the tool and try again. |
| POWER_ERROR_SLOW_DISCHARGE=
There seems to be excessive capacitance on VDD causing a slower system
discharge and shutdown. Consider minimizing overall capacitance loading
or use power from your target to avoid discharge delays. |
| POWER_ERROR_UNKNOWN=An unknown
power error has occurred. |
| POWER_ERROR_VDD_TOO_HIGH=The
VDD voltage desired is out of range. It exceeds the maximum voltage of
5.5V. |
| POWER_ERROR_VDD_TOO_LOW=The VDD
voltage desired is out of range. It is below the minimum voltage of
1.5V. |
| POWER_ERROR_VPP_TOO_HIGH=The
VPP voltage desired is out of range. It exceeds the maximum voltage of
14.2V. |
| POWER_ERROR_VPP_TOO_LOW=The VPP
voltage desired is out of range. It is below the minimum voltage of
1.5V. |
| PRESERVE_MEM_RANGE_ERROR_BAD_END_ADDR=Invalid preserve range end
address %s received. Please check the manual program ranges on the debug
tool's, "Memories to Program" property page. |
| PRESERVE_MEM_RANGE_ERROR_BAD_START_ADDR=Invalid preserve range start
address %s received. Please check the manual program ranges on the debug
tool's, "Memories to Program" property page. |
| PRESERVE_MEM_RANGE_ERROR_END_LESSTHAN_START=Invalid preserve range
received: end address %s < start address %s. Please check the manual
program ranges on the debug tool's, "Memories to Program" property
page. |
| PRESERVE_MEM_RANGE_ERROR_ENDADDR_NOT_ALIGNED=Invalid preserve range
received: end address %s is not aligned on a proper 0x%x address
boundary. Please check the manual program ranges on the debug tool's,
"Memories to Program" property page. |
| PRESERVE_MEM_RANGE_ERROR_STARTADDR_NOT_ALIGNED=Invalid preserve range
received: start address %s is not aligned on a proper 0x%x address
boundary. Please check the manual program ranges on the debug tool's,
"Memories to Program" property page. |
| PRESERVE_MEM_RANGE_ERROR_UNKNOWN=An unknown error has occurred while
trying to validate the user entered preserve ranges. |
| PRESERVE_MEM_RANGE_ERROR_WRONG_DATABASE=Unable to access data object
while validating user entered memory ranges. |
| PRESERVE_MEM_RANGE_MEM_NOT_SELECTED=You have selected to preserve an
area of memory but have not selected to program that area. Please check
the preserved ranges on the debug tool's, "Memories to Program" property
page, and make sure that any preserved memory is also designated to be
programmed. |
| PRESERVE_MEM_RANGE_OUT_OF_BOUNDS=The selected preserve range, %s, does
not fall within the proper range for the memory area selected. Please
check the manual program ranges on the debug tool's, "Memories to
Program" property page. |
| PRESERVE_MEM_RANGE_STRING_MALFORMED=The preserve memory range(s)
entered on the, "Memories to Program" property page (%s) is not
formatted properly. |
| PRESERVE_MEM_RANGE_WONT_BE_PROGRAMMED=Some or all of the preserve
memory ranges (%s) entered on the, "Memories to Program" property page,
do not fall under the indicated program range(s) (%s) for the memory
selected. Please check the preserved ranges on the debug tool's,
"Memories to Program" property page. |
| PROGRAM_COMPLETE=Programming/Verify complete. |
| PROGRAM_MEMORY=program
memory. |
| PROGRAM=program. |
| PROGRAMMING_DID_NOT_COMPLETE=Programming did not complete. |
| READ_COMPLETE=Read
complete. |
| READ_DID_NOT_COMPLETE=Read did
not complete. |
| RELEASEMCLR_FAILED=Release
from reset failed. |
| REMOVING_SWBPS_COMPLETE=Removing software breakpoints complete. |
| REMOVING_SWBPS=Removing
software breakpoints... |
| RESET_FAILED=Failed to reset
the device. |
| RESETTING=Resetting... |
| RUN_INTERRUPT_THREAD_SYNCH_ERROR=An internal run error has occurred. It
is advised that you restart your debug session. You may continue running
but certain run time features may no longer work properly. |
| RUN_TARGET_FAILED=Unable to
run the target device. |
| RUNNING=Running. |
| SERIAL_NUM=Serial
Number:\n |
| SETTING_SWBPS=Setting software
breakpoints....... |
| STACK=stack. |
| START_AND_END_ADDR=start address
= 0x%x, end address = 0x%x. |
| START=start. |
| TARGET_DETECTED=Target voltage
detected. |
| TARGET_FOUND=Target device %s
found. |
| TARGET_HALTED=Target
Halted. |
| TARGET_NOT_READY_4_DEBUG=The
target device is not ready for debugging. Please check your
configuration bit settings and program the device before proceeding. The
most common causes for this failure are oscillator and/or PGC/PGD
settings. |
| TARGET_VDD=Target VDD:
|
| TEST=test. |
| TOOL_IS_BUSY=ICD 4 is busy.
Please wait for the current operation to finish. |
| TOOL_VDD=VDD: |
| TOOL_VPP=VPP: |
| UNABLE_TO_OBTAIN_RESET_VECTOR=ICD 4 was unable to retrieve the reset
vector address. This indicates that no _reset symbol has been defined
and may prevent the device from starting up properly. |
| UNKNOWN_MEMTYPE=Unknown memory
type. |
| UNLOAD_WHILE_BUSY=ICD 4 was
unloaded while still busy. Please unplug and reconnect the USB cable
before using ICD 4 again. |
| UPDATING_APP=Updating firmware
application... |
| UPDATING_BOOTLOADER=Updating
firmware bootloader... |
| UPDATING_FPGA=Updating
firmware FPGA... |
| USE_LVP_PROGRAMMING=NOTE: If
you would like to program this device using low voltage programming,
select Cancel on this dialog. Then go to the Real ICE node of the
project properties and check the Enable Low Voltage Programming check
box of the Program Options Option Category pane (low voltage programming
is not valid for debugging operations). |
| USERID_MEMORY=User Id
Memory. |
| USERID=user Id. |
| VERIFY_COMPLETE=Verification
successful. |
| VERIFY_FAILED=Verify
failed. |
| VERSIONS=Versions. |
| VOLTAGES=Voltages. |
| WOULD_YOU_LIKE_TO_CONTINUE=Would you like to continue? |