7.1 Counter
Command
The Counter
command reads or increments the count value
of the monotonic counter. The counter value is stored in CSZ2. The maximum value of the
counter is fixed at 10,000. The starting value of the counter is programmed during
initial provisioning, and when the Configuration zone slot is locked, it cannot be
modified.
The counter is designed to never lose counts even if the power is interrupted during the counting operation. In some power loss conditions, the counter may increment by a value of more than one.
The counter can be attached to the HMAC key to limit its use. The counter will be incremented with the respective key until the counter reaches its maximum value, at which point the use of the key will no longer be permitted.
The number of legal uses for a key can be controlled by initializing the
Counter
to a nonzero value at configuration time. Contact Microchip
for details.